cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4Discovery GPIO

hillpatrickb
Associate II
Posted on May 14, 2013 at 23:40

I am trying to use GPIO Pin PE9 and PE10 as outputs to a system.  From using the STM32L1Discovery Board I know that the GPIO Output voltage should be 3 V.  But when I am using the F4 BOard my output on PE9 is 2 V and PE10 is 1 V.  When I make the pins low, I am reading 7 mV so I know that the pins are turning on, but does anyone know why I am only getting a 2V output?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 15, 2013 at 03:58

The pins don't have any other utilization on the board.

Consider how you have them configured.

Consider how they are loaded externally.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..