Posted on January 05, 2016 at 10:36Hi , I have the STM3240G-Eval board and currently I'm working on a project which in it I'll need to display text in the LCD. I searched the internet for some informations to configure STM3240G-EVAL LCD (MB785 driv...
Posted on October 22, 2014 at 11:41how get INEMO software demonstration, the server seem out of order, I try 6 times I receive, illegal character and after the server is out of order, try later
Posted on August 21, 2014 at 17:32I begin to use STM32xx_F4_HAL_DRIVER and I am looking for stm32f4_hal_discovery_debug.c. I use in my last project stm32f4_discovery_debug.c with standart Library. I should use stm32f4_hal_discovery_debug.c in a ...
Posted on May 14, 2013 at 17:31I have 3 STM32L152 discovery which anser ''Unknown target connected'' when I load a program from keil.I try setting BOOT0 HIGH when I push the reset Button .There no result.Best regardsYves de Brest
Posted on September 21, 2012 at 15:07Hi,I have 10 STM3240G-EVAL to make traing courses.On one board, I have load 2 programs too quikly ones behind the other. I cannot today load any program.I work with STlink2 and µvision4.Have-you any solution to...
Posted on January 06, 2016 at 11:36Hi HannibalThank you. I think that the TFT LCD interfacing with the high-density STM32F103_Eval is the same stm32F40G_eval but I have not idea to look for an application note.