STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429i-Discovery : USART issue & system_stm32f4xx.c

Posted on February 12, 2014 at 14:42Dear all, I am using the STM32F429i-Discovery, and I experience some problems with UART communication: received symbols are differents from TX. Discussing with some colleagues points out the baudrate might be in ...

stephane by Associate II
  • 2335 Views
  • 5 replies
  • 0 kudos

STM32F417 and LIS3DH SPI1 problem

Posted on February 13, 2014 at 22:59Hi forum!Here is a very strange problem I'm facing with the SPI1 peripheral of the STM32F417 connected to the LIS3DH. I have to single-step through my code with my debugger in order to get the right data from the ...

slal by Associate III
  • 2632 Views
  • 5 replies
  • 0 kudos

STM32F4 Discovery I2S DMA FIFO Error issues

Posted on February 08, 2014 at 20:52I'm currently testing  I2S between two F4 Discovery development boards.One board is master, running DMA, one is slave. Both are configured with the same sample set for verification purposes, so the data sent can b...

phil2 by Associate II
  • 2135 Views
  • 5 replies
  • 0 kudos

Problem with debugging

Posted on February 13, 2014 at 22:30Hullo , ...... Im working on Waveshare board (PORT207Z) , it has the STM32F207ZG chip , I can use the simulator debugger properly , but when I use my J-Link debugger , debugging does not work properly , it says (J...

SPI RX Buffer via DMA Too Big

Posted on February 13, 2014 at 14:07I've set up my DMA to transfer 106 half-words via the SPI to a memory buffer. I am quite confident that my buffer size is correct. However, when the transfer actually occurs, it is twice the size I expect (and is ...

jvavra by Associate III
  • 4611 Views
  • 15 replies
  • 0 kudos

ADC reference voltage of stm32f4-discovery

Posted on February 13, 2014 at 14:00I use stm32f4-discovery board. I am working with the ADCs, and for my prpose I need to set the ADC reference VREF+ at 3.2V. in the reference manual RM0090 it is said that stm32f4 LQFP100 has VREF+ VDDA pin. But th...

sen2 by Associate II
  • 2241 Views
  • 3 replies
  • 0 kudos

STM3240-G USB-MSC Wrong SD Card Size

Posted on February 12, 2014 at 18:03I'm using custom code which is somewhat ported from the STM3240-G USBD-MSC example application. I also made modifications to the read/write functions to take blocks as arguments vs. bytes. I've stepped through the...

nattayb by Associate II
  • 2182 Views
  • 4 replies
  • 0 kudos

ADC frequency

Posted on February 13, 2014 at 14:11Hi all,I'm using stm32f100c8 with an external oscillator 8MHz to produce a system clock of 24MHz. All the peripherals are on the default division lines.Now the ADC1 which is with the TIM1 on PCLK2 is supposed to r...

0690X00000602rGQAQ.jpg
sherif by Associate II
  • 1198 Views
  • 1 replies
  • 0 kudos

SPI raise/fall time

Posted on February 10, 2014 at 10:39HiI'm using STM32F373x SPI in slave mode. I get errors in about 0.1% bits transmitted, occurs in 50% of units from first production series of custom board. SPI lines have RC filter installed to improve EMC immunit...

bpacan by Associate II
  • 8381 Views
  • 11 replies
  • 0 kudos