STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA and CPU accessing SRAM same time

Posted on March 19, 2014 at 15:28Hi,I am working on a system using STM 32F107 processor(connectivity line). Because of our requirement same memory location of SRAM is accessed by both CPU and DMA. CPU is supposed to move the data from initial locati...

nmadhavan by Associate II
  • 11645 Views
  • 7 replies
  • 0 kudos

ADC regular channel not ready after enabling ADC

Posted on June 09, 2012 at 21:53I'm trying to use a single ADC channel on a STM32L151 using Keil Realview and ST libraries. After enabling the ADC I wait until the ADONS bit is set indicating the ADC is ready to convert but it does not set. Looking ...

bluscape by Associate III
  • 2205 Views
  • 6 replies
  • 0 kudos

Problem sending with USART_SendData

Posted on March 20, 2014 at 16:25 USART_SendData(USART1, 12); USART_SendData(USART1, v_dc_int); USART_SendData(USART1, v_dc_fra); If I send only one of the it is received fine. But if I send them all, I only can see the last of them. Do I...

pedroh44 by Associate
  • 1003 Views
  • 1 replies
  • 0 kudos

delay function Mcs o mls

Posted on March 18, 2014 at 22:06Hi, I'm looking how to perform a  delay function whith microsecondor milisecande Who can help me ?thank you alot

haythem by Associate II
  • 2819 Views
  • 8 replies
  • 0 kudos

ADC initailization problem on STM32L series

Posted on March 20, 2014 at 13:52Hi, I am trying to use ADC for reading the voltage on pin A4.. I wrote an initialization method, however it get stuck in the last WHILE. Here there is the code: void ADC_Initialize(void) {   ADC_InitTypeDef  ADC_Ini...

luca2 by Associate II
  • 1068 Views
  • 1 replies
  • 0 kudos

SIP Stack for STM32F4

Posted on March 19, 2014 at 10:19I want to build a VoIP Phone ith STM32F4. Does anybody know, if there is a small SIP-Stack that can easily used with microcontroller. Thanks Marc #cross-post

doebber2 by Associate II
  • 1813 Views
  • 2 replies
  • 0 kudos

SPI TI mode

Posted on March 19, 2014 at 10:49Hello,could somebody explain me what is TI mode in SPI? Thank you #ti-mode #spi

karolina by Associate II
  • 2566 Views
  • 2 replies
  • 0 kudos

General question about DMA

Posted on March 18, 2014 at 22:45Hello everyone, i have a few general questions about DMA and i will appreciate the help if someone could answer to my questions. I know it is used to transfer data at high speeds between memory and peripherals, or me...

arganasss by Associate II
  • 1435 Views
  • 2 replies
  • 0 kudos

DAC problem with STM32F4

Posted on March 17, 2014 at 18:51Dear All,I have tested the DAC example on the STM32F429 and I have understood the way using / driving the DAC on the STM32F4. I have tried to create my sample code using the STM32F429 Discovery template, but nothing ...