cancel
Showing results for 
Search instead for 
Did you mean: 

STM32_Init.c

mosine
Associate II
Posted on June 28, 2013 at 08:32

Hello. I want build a stm32_init.c for stm32f2xx micro. I try to find it, but nobody create it. And so, I need a aid to start. Can you help me?

Thanks
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on June 28, 2013 at 11:19

Hi Simone,

For which purpose do you need this file? May be you mean the ''system_stm32f2xx.c'' containing the ''SystemInit'' function and is available in the Standard Peripheral Library.

This library can be downloaded from ST page.

This is just a guess because it is not clear what do you need exactly.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.