STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Discovery USB OUT Report example

Posted on October 29, 2013 at 15:56Hello everybody, I'm looking for a working example using OUT Endpoint on STM32F4 Discovery board. I have no success with it. I modified Demo sample for an OUT Endpoint and Custom usage, and try to send one byte rep...

nihaoraja by Associate II
  • 2176 Views
  • 5 replies
  • 0 kudos

DMA won't get enabled

Posted on March 29, 2014 at 17:53 Hello stmGuys. I'm having a problem configuring my DMA. I've tried everything I can imagine and it still doesn't work. I want the DMA to transfer data from a memory array to the GPIOD->ODR register. Here is my DMA...

joecarlhr by Associate II
  • 3193 Views
  • 6 replies
  • 0 kudos

What triggers WFI exit?

Posted on March 30, 2014 at 08:39Hello,I want to use WFI, but I'm wondering how it works, what triggers the WFI to exit low power.I've defined systick for 1uSec (I'll use it later for some delays).I've defined timer2 for 100mSec.I need to do some ca...

zoharr by Associate II
  • 1511 Views
  • 1 replies
  • 0 kudos

Different triggers on the same clock

Posted on March 28, 2014 at 21:35 Hello, For a project I am working on I would like to generate interrupts on both edges of the HSI clock, for synchronization purposes. The sysclk is based on the main PLL, sourced from HSE. ...

matteo by Associate II
  • 5680 Views
  • 14 replies
  • 0 kudos

STM32F42X - TIMER + DAC + DMA: SINE WAVE

Posted on March 19, 2014 at 19:43Dear All,I would like to create a 1.5 MHz Sine Wave using TIMER + DAC + DMA.I have started from the DAC_SignalsGeneration example for Discovery board and then I have modified the TIM_TimeBaseStructure.TIM_Period  fro...

Low Power Myths

Posted on March 29, 2014 at 15:32I have some IoT application, where power gets quite critical. Comparing the current/MHz of different suppliers, I found the best STM32 in the STM32L0 line at about 80uA/MHz. Atmel proposes a pico-line with 70uA/MHz (...

flyer31 by Senior
  • 1190 Views
  • 3 replies
  • 0 kudos

DMA ADC Bit shift

Posted on March 29, 2014 at 09:18I am using DMA to transfer ADC data to a uint16 variable @ 1MS/s Than the value is shifted with another DMA channel to SPI and sent to an external DAC. Unfortunately the external 14 bit  ADC does not allow for left a...

fabio1 by Associate II
  • 1493 Views
  • 3 replies
  • 0 kudos

Parseable System Register Map

Posted on March 29, 2014 at 00:40Is anyone aware of any documentation that contains an easily parseable system register specification for an STM32 MCU that one could use to generate code, documentation, etc... from?  Something like the reference man...

mfranklin by Associate III
  • 554 Views
  • 0 replies
  • 0 kudos

DAC for sweeping frequency of Sine wave

Posted on March 28, 2014 at 16:42I want to generate sine wave (single cycle) and then change the frequency using DAC. basically Sweep the frequency... How would I do that.Thanks for your help in advance.     #stm32f4

Clock generation from 14.7456MHz

Posted on March 26, 2014 at 11:26In the user manual: AN2606 - STM32 microcontroller system memory boot mode it describes that when using a 14.7456MHz clock crystal the bootloader configures the PLL to run at 48MHz. How is this achieved? What setting...