2013-07-22 12:34 AM
RM0316
15 Operational amplifier (OPAMP)
Table 54. Connections with dedicated I/OOPAMP1 inverting input: PA3 (VM0)PC5 (VM1)
15.4 OPAMP registers
15.4.1 OPAMP1 control register (OPAMP1_CSR)Bit 8 VMS_SEL:0: PC5 (VM0) used as OPAMP1 inverting input1: PA3 (VM1) used as OPAMP1 inverting inputOPAMP2, OPAMP3 and OPAMP4 have the same errors.2013-07-23 2:02 AM
Hello,
Thanks for this feedback. I checked the issue you reported & confirm it for OPAMP1, OPAMP2 and OPAMP3. For OPAMP4 there is no issue. The correct information is in the registers description. So, the table 54 needs to be fixed. This will be done in next reference manual release. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.