STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 compiled code addresses at 0x0 not 0x08000000

Posted on July 15, 2014 at 14:57Hi all,I saw that the current practice is to compile all code at 0x08000000 offset. This is fine for me, but now I have an application with a lot of constant tables in flash, and more important, a ''host'' application...

raimond by Associate III
  • 2493 Views
  • 3 replies
  • 0 kudos

GDB became very slow in CoIde

Posted on July 15, 2014 at 12:03 Hi everyone, I'm working on a STM32F427 with CoIde on Windows Vista for a long time now without any issue. Since yesterday my debugger became very slow, very very slow. when i hit the ''pause'' button it takes approx...

benoit2 by Associate II
  • 1697 Views
  • 3 replies
  • 0 kudos

DMA2 problems: NDTR not zero

Posted on July 09, 2014 at 18:40I'm having some problems with DMA transfers apparently stalling on our STM32F405ZGT6 board. The problem seems to only happen when I have multiple streams running. So, I have Stream3 using SDIO, with 32 bit wide access...

STM32F3 Discovery power circuit heating up

Posted on July 14, 2014 at 00:01I was testing my STM32F3Discovery with an external 5V power supply (generic 5V 2A wall plug), and after about 30 seconds it stopped operating (LED flashing demo stopped flashing), and soon after I smelled something bu...

Dual Mode Bluetooth Stack options for STM32

Posted on July 14, 2014 at 14:35Hi All,I am new to MCu development and looking for dual mode bluetooth stack options that have been successfully ported to STM32 or any other STM MCUs.I am looking for following std profile support :1) BT : HFP (HF ro...

aashish by Associate
  • 2096 Views
  • 2 replies
  • 0 kudos

Fully Open Source Educational Nucleo-Based Robot

Posted on July 15, 2014 at 02:30Hello everyone,My name is Abe Howell and I would like to share my latest open source robot project, Apeiros.https://www.kickstarter.com/projects/477229692/apeiros-the-next-generation-open-source-robotApeiros is built ...

abe by Associate
  • 1121 Views
  • 0 replies
  • 0 kudos

STM32 SPI Hardware CS

Posted on July 01, 2014 at 12:40Hello,I'm using a STM32F30x as a Slave. The Master is  a custom board that select/deselect the Slave by toggling an output pin. In the Slave side i configured the SPI with hardware management, SPI_InitStructure.SPI_NS...

khalid2 by Associate II
  • 2140 Views
  • 3 replies
  • 0 kudos