cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 USB VCP receives only byte by byte

lauris
Associate III
Posted on January 17, 2014 at 13:08

Hello,

Maybe anyone have met with situation or have any hints where to look for problem if I receive data in ''EPx_OUT_Callback()'' function only by one byte, even if it was sent significantly larger amount of it.

USB irq handler is taken from V4.0.0 USB-FS-Device library - ''VirtualComport_Loopback'' project.

Everything else seems to be working fine - performance not yet tested, device is recognized, using ''CDC_Send_DATA()'' function data to PC is transmitted in packets up to 63 bytes per packet. Bet when it comes to receiving info sent by PC - in ''EP3_OUT_Callback()'' I receive only packets of len == 1, if string sent from PC is longer than 1B it is received only as multiple transmissions of len == 1.

Any offers where to start looking for problems?

Laurynas.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0