STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32_Programmer_CLI fails to flash

Using the STM32 CLI on Windows:STM32_Programmer_CLI.exe c port=swd reset=HWrst -e all -d my_filename.hex -v -s -g This just prints: If I remove the -d option, it performs the erase, so I know it can talk to the chip.  I have tried the verbosity optio...

JBill10_0-1731965731898.png
JBill.10 by Associate III
  • 785 Views
  • 1 replies
  • 0 kudos

Resolved! RCC stuck!

hey thereI have a customized board with STM32F030K6T6 on it and a 11.0592MHz crystal for HSE. the thing is my code does not run through and when I try to debug it, I can see it sticks in SystemClock_Config(), more specifically, in HAL_RCC_OscConfig()...

Ala by Senior
  • 5085 Views
  • 8 replies
  • 2 kudos

Resolved! Question about SAR ADC in STM32H753

Questions:1. Does STM32H753 have three independent 16-bit SAR ADC modules?     Any other STM32 parts also have 16-bit SAR ADC modules?2. Can a selected channel in each 16-bit SAR ADC module (Totally 3 selected channel in the 3 modules) be sampled sim...

Resolved! Shifts in conversion data from ADC on STM32H7B3

Hi!We are characterizing the ADC's in the STM32H7B3 µc. During temperature cycling of the HW we are observing some unexpected shifts in the conversion data from the ADC. The phenomena is observed across multiple HW units in varying degree. From one p...

HansPLJ_1-1731599396212.png HansPLJ_3-1731599807259.png HansPLJ_2-1731599466111.png
HansPLJ by Associate III
  • 3964 Views
  • 9 replies
  • 6 kudos

Resolved! Delay, multi milliseconds, on the STM32F0, again..

where I wrote it among the codes.. // Here I have to wait 500ms.Can you help me to prevent the timers from being affected by this wait?Can you give me the codes that I will add. Because I am very confused..I tried many things but they all stopped the...

XooM by Senior
  • 20599 Views
  • 70 replies
  • 15 kudos

Resolved! GPIO_Analog pin without ADC connection?

Hi,on the STM32U5G9VJT6Q, when I click on many pins such as PD5 (screenshot below) it shows GPIO_Analog but there does not seem to be any ADC channels (or other analog functionalities) connected to it.What does setting it to GPIO_Analog do?Can I stil...

Ricko_0-1731894166741.png
Ricko by Senior III
  • 1135 Views
  • 2 replies
  • 2 kudos

Resolved! SPI interface to LCD with DMA

I'm using SPI on STM32H563 with DMA to interface to a ST7789 LCD controller.  During the LCD initialization I'm using a loop to send a series of command/data bytes using the HAL_SPI_Transmit_DMA() HAL function but the DMA status never goes back to RE...

PFlor.2 by Senior II
  • 3387 Views
  • 3 replies
  • 0 kudos