User Activity

Hello,We are using the MCU STM32H745 in our current design.We have faced the issue of working MCU properly and below are the problem,Case 1 : At power ON, some time the MCU work properly and sometime does not work properly, when it is not work proper...
Hello,In my current project, we are using MCU - STM32H745Xi and integrated with SDRAM - IS42S32800J-7BLI.As of now, we are accessing 3 location of SDRAM to write and read the data and below are the observations:When we write the data and read it imme...
Hello,We are using the  Part#STM32H745XIH6 in our current product and it is going to be use in production.We are very near to release the product but at last we are facing the issue in the SD Card communication and below are the details.At power ON, ...
Hello,I am using the MCU : STM32H745XIH6 in my currnet product from last couple of the years and it is working fine till.Recently, we face the issue in I2C line.I2C3 line connected with,Super capacitor Board through connector(there is I2C IO expander...
Hello,I want to use STM32F439BG in my product.I am Confusing about the LCD Display.I want to use LCD - Capacitive Touch, 5.7 Inch, RGB (R-8, G-8, B-8, HSYNC, VSYNC, CLK, DE) which will be connected with STM32F439BG.Please suggest the LCD Compatible w...
Kudos from