User Activity

Hi,What happens if I want to use high side driver this way: Thank you,Tim
 Hi,I have been trying to place a function in the ITCM region for some time with no luck. As close I get was HardFalult There are some examples for the F7 series on the web. Some dating back to 2016, some similar to F767 with the same core but I cann...
Hi,Anyone having problem connecting STLINK on NUCLEO-H503RB board?I have two boards not showing up in device manager (both W10 and W11 PCs). Tried different PCs, cables and result is the same: LD7 LED is not lit, LD1 red lit, green pulsing, LD3 not l...
Hi,I am having uart baudrate problems while HSI clock as uart source clock. No problem with PCLK as source with the same uart. In Cube IDE (V1.16.0) and F7 software package (V.17.2), I get different values for HSI_CALIBRATION:Ide gets as 0x10 while r...
Hi,Updated from 2.15 today. Having DFU download problem seen attached.Board is recognised but upper right still stated as "Not connected" and download fails.Downgraded to V2.15 and same board connects and downloads OK. OS: W10 64bitBoard: STM32F767NI...