Hello, I made a board with STM32G030J6 in SO8 package. There is not much pins so I need to use UART bootloader. Problem is that BOOT0 is on the same pin as USART.I have USB-3V3_UART so I connect BOOT0 to 3V3 first, start the power supply, then I reco...