STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use I2C to ignore NACKs? (stm32f401 vs. SCCB)

Posted on August 05, 2014 at 15:12HiI'm trying to interface an OV7670 module using STM32F401 discovery board. First step is to get this SCCB interface going, which seems to be an I2C ripoff, http://www.ovt.com/download_document.php?type=document&DID...

bgeri91 by Associate
  • 1004 Views
  • 0 replies
  • 0 kudos

STM32F401RE SPI Init without CMSIS Functions

Posted on July 22, 2014 at 10:53 Hello, I have a problem with the initialization of the SPI1 from my STM32F It doesn't work and I don't now what I doing wrong or what I forged. When I write something in the data Register ( SPI1->DR), nothing h...

c239955 by Associate
  • 1452 Views
  • 3 replies
  • 0 kudos

Bugreport Cube32MX 4.0 & HAL_UART_TxHalfCpltCallback

Posted on August 02, 2014 at 08:21Hi,In the HAL documentation, stm32fxx_hal_uart.c & .h, I can read that in interrupt mode, the HAL_UART_TxHalfCpltCallback is called after half of tx is transfered but this is wrong.The HAL_UART_TxHalfCpltCallback is...

Osto by Senior
  • 615 Views
  • 1 replies
  • 0 kudos

I2C Address Issue

Posted on August 05, 2014 at 07:53Hi All, I am having an issue with I2C on the STM32F4. After successfully transmitting an address byte with values below 0xF0 , but when address value is more or equal 0xF0  (e.g. 0xF0, 0xF2, 0xF4 ..) - the slave ack...

0690X00000602stQAA.jpg 0690X00000602w6QAA.jpg 0690X00000602wBQAQ.jpg

Help with simple ADC on STM32F4

Posted on July 17, 2013 at 16:46 Hi all, I'm trying to get a simple ADC working on the stm32f4 discoveryboard. At the moment I simply want to obtain an input value(ConvertedValue) as a variable rather than saving to memory inDMA. I'm struggl...

F429 Serial Audio Interface hardware examples?

Posted on August 04, 2014 at 13:33Are there any reference designs or documents which show the SAI in use with TDM capable parts such as the Cirrus CS4244 (4In/4Out) ?Many thanks. #sai-audio-codec

g4 by Associate
  • 1213 Views
  • 2 replies
  • 0 kudos

Error: __vector_table not found when dowloading

Posted on January 29, 2013 at 05:28Using STM32F103ZE and IAR Embedded Workbench IDE 5.4 using assembler (no C). The program assembles and links with no errors. When selecting ''download and debug'' option the following errors occur: Warning: __vecto...

sue by Associate III
  • 4837 Views
  • 5 replies
  • 0 kudos

DMA2 never triggers interrupt on ''transfer complete''

Posted on August 04, 2014 at 12:05Hi all!I'm trying to configure DMA2 to trigger an interrupt on ''transfer complete'' event. I'm using DMA2 to transfer data from ADCs to memory. However, it seems that DMA2 never triggers an interrupt, but data is t...

marko2 by Associate II
  • 4657 Views
  • 9 replies
  • 0 kudos

PROBLEMS WITH STM32F107 + DP83848

Posted on August 03, 2014 at 00:32Hello! We are working in a product that comunicate with other equipments over ethernet interface over tcp/ip protocol, all works fine but sometimes something happen and just ethernet peripheral stop, all other perip...

paveglio by Associate II
  • 1634 Views
  • 3 replies
  • 0 kudos

X-NUCLEO-IDB04A1

Posted on May 28, 2014 at 01:16Hey,Where can I get this? I live in canada and currently have the other blueNRG dev board, but would like to get my paws on this.Also, how much ram do I need to dedicate to the bluetooth to practically get around the u...

johnlee by Associate II
  • 1611 Views
  • 3 replies
  • 0 kudos