STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What does IOPORT mean?

Posted on August 01, 2014 at 21:40In the memory map (Figure 2, page 45, RM0091 Rev 6), a region of memory is depicted at 0x50000000 - 0x50001fff; this region is labeled IOPORT.  However, I could not find any other reference to that in the entire Ref...

rgrimes by Associate II
  • 874 Views
  • 1 replies
  • 0 kudos

STM32F0 discovery board with I2C

Posted on August 02, 2014 at 18:40 Hello, I want to communicate with an I2C eeprom but I don't know how to read/write bytes and how to sen the adress. I have an initialisation code that I found on the forum but I am stuck. does anybody now ho...

What is hardfault?

Posted on August 04, 2014 at 09:14My system was under hardfault in doing some job without saying anything. What is hardfault? which one make hardfault in stm32f407ve. Thanks ahead. Kevin

yiulsup by Associate II
  • 1038 Views
  • 1 replies
  • 0 kudos

rtc & stm32f429

Posted on August 03, 2014 at 19:10hello every one i need to use lse for rtc clock src. because i want it still working at the power of( with vbat)my lse circuit work correctly because i use the mco1 as lse clock src and i have 32.768 khz this pin (p...

please give me the solution for resolving the error

Posted on August 01, 2014 at 20:51Hi sir/madam                when I am compiling my code for tcp/ip echoserver and echoclient I am getting the error error: storage size of 'echoServAddr' isn't known. I am compiling the code by using CooCox CoIDE To...

Double buffered DMA Interrupt not working

Posted on August 02, 2014 at 10:01Hi All, New to the STM32 so please bare with me.... I have setup timer4 to generate a sinewave modulated PWM using double buffered DMA and that works very well, I can see my waveform on the pin and it contains the c...

bmentink by Associate II
  • 1256 Views
  • 2 replies
  • 0 kudos

Flash loader demonstrator not working. stm32f407-disc

Posted on August 01, 2014 at 13:50Hello everybody I am trying to disable read out protection (level 1) on my stm32f407-discovery with flash loader demo (v2.6). I've connected Boot0 to Vdd, PB2 (boot1) to Gnd and my serial port (via max232) to usart1...

Upgrade problem with STM32F4-Eval

Posted on February 06, 2013 at 10:43Hello,I've a problem with my STM3240G-Eval board and my development tool chain. I use Atollic or Keil �Vision demo. When I want debug my program or ST examples, the development software send me ''Old ST-LINK firmw...

Nucleo F0: Problem with I2C

Posted on August 01, 2014 at 15:59 I2C_HandleTypeDef hi2c1; int main() { HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_I2C1_Init(); HAL_I2C_Init(&hi2c1); if(!(HAL_OK == HAL_I2C_IsDeviceReady(&hi2c1,0x39,1,1000))) __ASM(''NOP'');...

mfkfx by Associate II
  • 3028 Views
  • 5 replies
  • 0 kudos