cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L152 OPAMP Output current?

Tom
Associate II
Posted on February 05, 2014 at 18:41

Hi All!

I would like to use the  STM32L152  Opamp output pin to pulse drive the MOC3020 optotriac.

The pulse current should be ca 15mA-20mA for the optotriac to fire up under any temp. conditions.

Can I source this amount of current form the opamp pin or is it just like any other GPIO pin?

thanks and regards

Tom

   

#stm32l152-opamp
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
raptorhal2
Lead
Posted on February 05, 2014 at 21:24

The data sheet for the uP defines drive current capability. The comparator comes up substantially short of your requirement. Same problem with the DAC even with it's internal buffer amplifier. Use an extrernal buffer amp.

Cheers, Hal

Tom
Associate II
Posted on February 06, 2014 at 12:27

Thanks Hal!