User Activity

I have just changed from STM32F (works fine) to STM32H and have used MX to generate the Code for a SRAM 16 bits wide and 6 Address lines. The FMC outputs the NE clock but depending on the Data Bus Setting 8, 16, or 32, NE produces either 8, 4, or 2 C...
Posted on February 13, 2017 at 16:30I am currently running CAN1 and CAN2 on the F427 and need to check/validate the Transmitted Data.Both CAN1 and CAN2 function correctly.I wish to Transmit Data on CAN1 and, if possible, Receive the sent Data in the...
Posted on September 15, 2016 at 17:40STM32CubeMX 4.16  STM32Cube FW_F4 V1.13.0 I have CAN working OK and need to get the Error Status, I have the following Code fragment but do not receive an Error Code when a CAN Error occurs i.e. disconnected.    ...
Posted on September 13, 2016 at 13:41STM32Cube FW_F4 V1.13.0 I have a board using CAN1, CAN2, SPI_1 and SPI_2 All functions work independantly fine CAN1 and CAN2 work in Polling mode and Interrupt mode. SPI_1 and SPI_2 work OK in polling mode using ...
Posted on August 26, 2016 at 10:31I am curently using the STM32F407 and F427 MicroControllers. Can anyone advise if they are CAN FD compatible or if this is a software layer etc. Any information would be helpful. Rgds John W
Kudos from