User Activity

Posted on February 06, 2014 at 09:26Hello together, i´ve been searching for information about the minimal voltage wich has to applied to Vref-. In particularly it is around the stm32f103CBT6. I´ve used the search function in the RefManual, but co...
Posted on August 10, 2013 at 09:28Hello together, i´m just asking in case someone had the same issue and knows the answer - of course i don´t want u to read the manuals for me... So, i´m using the PWM input feature on Timer2 and in general it wo...
Posted on April 15, 2013 at 19:55Hello Community, i´m having a stm32f3Discovery under the Keil´s µVision4 Compiler programming in c++. I got to the point, where i could use the ''NEW''  operator. To be honest, i have no idea, what is really goin...
Posted on April 12, 2012 at 10:13Hello there, i have downloaded the ''STM32_USB-Host-Device_Lib_V2.1.0'' library, installed the VCP driver and the VCP USB_Device_Example works on the MCBSTM32C board ''out-of-the-box''. Great thing at this point! As...