STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Discovery not working out of the box.

Posted on July 23, 2012 at 19:53I got 2 new STM32F4 Discovery boards and both are not being recognized by STLINK utility. Here some of the observations. I compared the behavior to STM32F1 discovery board. (It is Windows 7 PC).1) Plug in STM32F1 boar...

bsp0524 by Associate II
  • 6184 Views
  • 15 replies
  • 0 kudos

STM32F4Discovery RTC WakeUp Interrupt

Posted on August 17, 2014 at 15:34 Hello,I'm currently quiet frustratedI'm trying to set up with the RTC wakeUp register an interrupt of 128Hz. For the RTC the LSI is used (I know not very precisely but for current testing propuse its enough)here i...

SRAM_DataMemory Issue

Posted on August 13, 2014 at 10:55Hi, I am unable to run the example STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\FSMC\SRAM_DataMemory on my STM3210E-EVAL Board. Although I have made the following settings Project->Options ...

Simple Question on Ethernet Boundary Addresses

Posted on August 18, 2014 at 08:50In the STM32F407xx Datasheet (Doc ID 022152 Rev 4) Table 10 ''STM32F40x register boundary addresses'', there are 5 base addresses listed for the Peripheral ETHERNET MAC. How do these base addresses correspond to th...

wjthomas by Associate
  • 1186 Views
  • 3 replies
  • 0 kudos

Encoder configuration giving erroneous speed

Posted on August 16, 2014 at 13:49Hi, I am trying to measure the rpm of a geared DC motor. The manufacturer claims a speed of 500rpm at 12V but my calculations give a speed of around 1600rpm! The gear ratio is 19:1. I have written the following code...

furqan by Associate II
  • 2151 Views
  • 4 replies
  • 0 kudos

Multiple UART Problem ! !

Posted on August 14, 2014 at 12:43The original post was too long to process during our migration. Please click on the attachment to read the original post.

How to change the CPU with STMCube

Posted on August 14, 2014 at 23:09Hi,I have a project with STM32F417 and want to change it to SMT32F407.I cant find any way to change the CPU.How can I change without enter all information again into STMCube?Tkans for you help.

Osto by Senior
  • 1395 Views
  • 4 replies
  • 0 kudos

inverted uart input

Posted on August 17, 2014 at 02:04Hi, I have a device which is sending an inverted UART on the line. The startbit is 1, the stopbits are 0. The whole line is inverted, but the other syntax of uart is right. So is there e possibility for receiving th...

Using DMA to load TIMx CCRy

Posted on August 16, 2014 at 22:34I'm trying to find an example of loading the next timer delay via DMA.  I want to sweep a square wave over a range of frequencies and this looks as if it might be able to do it very neatly. Assembly preferred as I'm...