STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 input output PWM program

Posted on August 14, 2014 at 23:58HiI'm programming this code. It should read a PWM input then ouputs 4 different PWM after calculation based on the input. I've successfully programmed 2 different code: one for the input and one for the output. They...

louis23 by Associate
  • 1596 Views
  • 1 replies
  • 0 kudos

SPI timing

Posted on August 14, 2014 at 23:44I am writing an SPI interface where after 4 messages are sent I toggle a pin.  My issue is my pin is toggling before the transmission is complete(I can see my pin go high after the 3rd message).  I am monitoring the...

ebommer by Associate II
  • 1148 Views
  • 1 replies
  • 0 kudos

STM32 & CAN bus - problem with communication

Posted on March 24, 2014 at 19:33I have STM32F429-Disco board and I'm trying to connect two CAN interfaces, which this board has.   My parts of the code are: /* CAN1 init function */ void MX_CAN1_Init(void) {   hcan1.Instance = CAN1;     hca...

anulka by Associate
  • 4776 Views
  • 7 replies
  • 0 kudos

STM32L151 bricked after attempting USB

Posted on August 14, 2014 at 14:13I have about 5 different projects using STM32 F series and 2 using STM32L151 on custom board.   I use the ST-link V2 to program and debug them.I was attempting to get a custom board with USB port working.  I loaded ...

STM32F400 USART NVIC_Configuration

Posted on March 25, 2014 at 17:51The original post was too long to process during our migration. Please click on the attachment to read the original post.

afduarte by Associate II
  • 1577 Views
  • 4 replies
  • 0 kudos

Interference of DAC output and the PWM

Posted on August 13, 2014 at 07:21Hello,         I am generating a signal which goes to output of the DAC, but unfortunately when I use the PWM module of the system the PWM signal frequency distorts the signal generated by the DAC.Can anyone tell me...

False Framing Errors?

Posted on August 03, 2014 at 23:35I am using an STM32F407 to receive data via UART and seem to be getting false FE interrupts. There are two reasons why I believe that they are false: I have looked at the timing on an oscilloscope and it appears t...

dibs by Associate II
  • 1832 Views
  • 5 replies
  • 0 kudos