STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using I2C Interface for MDIO (SMI / MIIM)

Posted on September 15, 2014 at 20:49I have an application where I need to manage a SW that my micro does not have a data interface on.  The switch uses MDIO as the interface for management (not just for PHY configuration).  Has anybody used a I2C p...

mvonahnen by Associate III
  • 3111 Views
  • 1 replies
  • 0 kudos

spi in stm32f103

Posted on September 15, 2014 at 16:55hi every bodyim trying to use spi cmsis function in STM32F10x Standard Peripherals Library V3.4when i use examples of its own folder my compiler keil5.11a (with stm periph lib v3.5) shows this error:and i know th...

0690X00000605A0QAI.png
mhdizgah by Associate II
  • 908 Views
  • 1 replies
  • 0 kudos

STM32F429 timer debug question

Posted on September 14, 2014 at 20:03Hello friends.I use EWARM as IDE. The platform is STM32F429I-DISCONow I study timers' behavior. When I use one step through the code while debugging (Step Into in the EWARM) the value of the CNT register changes ...

baev_al by Associate III
  • 1208 Views
  • 4 replies
  • 0 kudos

STM32F405, rtc issue

Posted on September 13, 2014 at 02:22Dear all, i connected a 32.768Khz quartz to the external clock source (PC14, PC15), i would like to have an interrupt generated each second, for the system clock. Also, i connected a battery between VBAT and gnd,...

Angelo1 by Associate II
  • 1371 Views
  • 3 replies
  • 0 kudos

SDD1963 LCD Controller with FSMC

Posted on March 11, 2013 at 20:21Hello, Does anybody already used sdd1963 lcd controller with STM32 through FSMC? The used code to configure the FSMC is: void FSMC_LCD_Init(void) {   FSMC_NORSRAMInitTypeDef  FSMC_NORSRAMInitStructure;   FSMC_NORSRAM...

gsilva by Associate II
  • 2440 Views
  • 4 replies
  • 0 kudos

STM32L0 MCU EEPROM write

Posted on July 29, 2014 at 14:44Hi.I use Nucleo board with STM32L0x3 MCU. There are special sequence for EEPROM TYPEPROGRAM_BYTE process? I can write 4 bytes data (TYPEPROGRAM_WORD) but can't write 1 byte data (TYPEPROGRAM_BYTE):uint32_t Address = 0...

STM32F205 flash self programming

Posted on September 06, 2014 at 22:11Hello, First, sorry for my poor english.I have a problem with a STM32F205. I am trying to read the content of flash memory , and for some bytes i have a value different with my firmware binary file. But the appli...

msstaf by Associate
  • 1310 Views
  • 2 replies
  • 0 kudos

What is the default PriorityGroup setting if I didn't call NVIC_SetPriorityGrouping or NVIC_PriorityGroupConfig

Posted on September 13, 2014 at 22:14I'v found in the Cortex-M4 file that the default value of PRIGROUP is 0. while the legal value of STM32 is from 3 to 7. And I didn't find the PRIGROUP set in startup file or system_stm32f4xx.c. What is the defaul...