STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Understanding ADC Sampling

Posted on September 16, 2014 at 06:30I have a simple operation to perform with the STM32F4 (on a Discovery board) but the solution escapes me. Mostly from the fact that, even after looking at sample code and reading the manual, I don't quite get it ...

stm32439i-eval2 LCD usable definition ?

Posted on September 11, 2014 at 16:38Hi, I was wondering why in the stm32439i-eval2 dev board, the am640480G5TNQW  LCD is configured to be used in a 480x272 (unusual) defnition. Is it possible to use it at 640x480 as part of driver allow it ? Moreo...

gilberce by Associate II
  • 1238 Views
  • 2 replies
  • 0 kudos

STM32L0 snippet - cmsis rtos

Posted on September 03, 2014 at 03:23Hi all, I am using the STM32L0 snippets code and would like to use the CMSIS RTOS which is included inside in the form of cmsis_os.h. Inside Truestudio, I added the header file and included the folder inside my ...

jephua by Associate II
  • 2927 Views
  • 5 replies
  • 0 kudos

Advanced Timers not working in PWM in all channels.

Posted on August 01, 2014 at 02:25Greetings,I'm attempting to use stm32cubemx to configure the timers of a stm32f427ig to control a few rgb leds as open-drain, pwm outputs.  I'm using timers 1,3,4,5, and 8.  All of them are using channels 1 thru 3, ...

STM32F407IEH6 - I2S2_MCK and I2S3_MCK

Posted on September 15, 2014 at 17:21Hi everybody!We are currently working on some audio related project. We are using TI's ADC (PCM4201) and DAC (PCM1748) on our board and we will communicate with them using I2S. Now, we have to select appropriate ...

LIS3DSH Examples

Posted on September 16, 2014 at 08:04Hi, I am a beginner in STM32F4 Discovery. I am using STM32F4 Discovery MB997C board. The firmware STM32F4-Discovery_FW_V1.1.0 contains example for LIS320DL. But my board has LIS3DSH mems accelerometer. Is there a...

Delay with timers on stm32F107

Posted on August 28, 2014 at 11:52HiI am working on STM32F107 evaluation board, There is a need for me to implement a delay in ms using H/W timers with polling method. I looked for other examples but they are not working for me can anyone suggest me...

sajeed by Associate II
  • 2484 Views
  • 4 replies
  • 0 kudos

Programming STM32F103 discovery controller via UART1

Posted on September 15, 2014 at 13:13Hi, I am trying to program the standard STM32F1 discovery board (STM32F103 controller) through usart1 (without using the stlink debugger integrated within the board). I have removed 2 jumper associated with CN2. ...

aruns06 by Associate II
  • 1420 Views
  • 2 replies
  • 0 kudos

STM32F051K6 NVIC_SetVectorTable

Posted on June 13, 2013 at 06:26Dears,Do STM32F0 support NVIC_SetVectorTable command?I would like to point the vector table as my program start from 0x08001001NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x1000)Thanks.

ricky by Associate
  • 2080 Views
  • 4 replies
  • 0 kudos