cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f405, help on jtag programming

Angelo1
Associate II
Posted on March 06, 2014 at 00:08

Dear all,

i am trying to program a stm32f405 just soldered on a prototype pcb.

Seems jtag TAP is accesible, but for some reason i cannot halt the cpu:

Open On-Chip Debugger 0.7.0 (2013-08-04-10:13)

Licensed under GNU GPL v2

For bug reports, read

        http://openocd.sourceforge.net/doc/doxygen/bugs.html

Warn : Adapter driver 'parport' did not declare which transports it allows; assuming legacy JTAG-only

Info : only one transport option; autoselect 'jtag'

parport port = 0x0

adapter speed: 1000 kHz

adapter_nsrst_delay: 100

jtag_ntrst_delay: 100

cortex_m3 reset_config sysresetreq

Info : clock speed 500 kHz

Info : JTAG tap: stm32f4x.cpu tap/device found: 0x4ba00477 (mfg: 0x23b, part: 0xba00, ver: 0x4)

Info : JTAG tap: stm32f4x.bs tap/device found: 0x06413041 (mfg: 0x020, part: 0x6413, ver: 0x0)

Info : stm32f4x.cpu: hardware has 0 breakpoints, 0 watchpoints

> halt

target was in unknown state when halt was requested

Halt timed out, wake up GDB.

Invalid ACK 0 in JTAG-DP transaction

in procedure 'halt'

> flash info 0

device id = 0x00000000

Cannot identify target as a STM32 family.

auto_probe failed

in procedure 'flash'

I exclude ''programmer'' issues, i already used it succesfully in other cortex_m.

I am not using NJTRST wire, hope is not an issue.

I have a suspect i could have damaged the cpu while soldering it.

Every help is really appreciated.

Regards

Angelo

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on March 06, 2014 at 04:21

>Info : stm32f4x.cpu: hardware has 0 breakpoints, 0 watchpoints

Some thing wrong there.

What about NRST? What pins have you got wired up, and how?

>I have a suspect i could have damaged the cpu while soldering it.

Honestly most everything I see here is shorts and opens, and a few getting PIN 1 orientation wrong.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Angelo1
Associate II
Posted on March 07, 2014 at 00:20

Dear clive1,

many thanks, i am still stucked and can't program the chip in any way

i have no pin 1 orientation issues, and also, checked all VDD and all VSS, they are connected correctly to the chip.

I also replaced the chip, same exact result.

I have seen that in my schematic i don't have connected BOOT0 pin (unconnected), can this be an issue ?

I also read that this chip shouldn't need any NJTRST connected.

So i connected only

JTCK -> pin 76

JTDI -> pin 77

JTDO -> pin 89

JTMS -> pin 72

I pulled them all up with 10K on the board.