STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

inconsistent Calibrations values.

Hi.. Can anyone tell me why the ADC Calibration value is not the same before and after I initialize the DACIt seems that the value maxes out if I calibrate after I have initialized the DAC.The calibration register is 7 bits.The ADC also measures inco...

DAC_ADC.jpg
spa23 by Associate III
  • 2261 Views
  • 4 replies
  • 0 kudos

Resolved! Reading data with BRS on fdcan line

  I am using STM32H5RE23T6. I implemented the function of receiving data from the FDCAN line. When I select FDCAN mode without BRS, it works without any problems. When I select with BRS mode.I set the arbitration phase to 1mbps.I set the data phase t...

CANZT-FD by Associate III
  • 3042 Views
  • 6 replies
  • 1 kudos

Resolved! USART used as GPIO to send break signal for DMX-512

Hello!I am just getting started with STM32 universe. I've already finished my first project using the IDE SW4STM32 and I board I've designed using the STM32F070CBT. I've also used STM32CubeMX to generate the basic code.I wanted to keep using this boa...

Resolved! Parallel TFT Display not working

Hello Guys, Currently I am using Parallel RGB888 TFT display with resolution 800X480 in which I am using STM32F429ZIT6 controller using LTDC with DMA2 and I am printing whole RED color on display but display showing lines. My question is as I am not ...