Question
Need suitable External Flash Loader - STM32F423ZHT6 GD25S512MDYIGR
- July 25, 2024
- 1 reply
- 1087 views
Hi,
I'm creating a project on GUI using an embedded wizard. While I'm trying to flash the code to my STM32F423ZHT6 custom board. It shows an error: failed to erase memory.
I'm using STM32CubeProgrammer and I successfully erased the entire flash. But still it shows the same error. I'm using GD25S512MDYIGR QSPI Flash memory. So I need a suitable flash loader for the STM32CubeProgrammer.
Regards,
Meenakshi.