STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Rotate screen 90 degree

Posted on August 30, 2014 at 00:00Dear Sir / Miss I need the screen look length>width, need to rotate screen 90 degree. Please help #ask-smarter-questions

Linda by Associate II
  • 1003 Views
  • 3 replies
  • 0 kudos

program stuck in if(true) condition

Posted on September 22, 2014 at 20:36hi all, i work with stm32f4 and keil uv5 my program seems stuck in if condition my code is while(1)         {             if(i==0)             {                 break;             }         } and my debugger say...

STM32F101/103 VBAT Monitoring

Posted on September 22, 2014 at 12:33I have a lithium battery connected to the VBAT pin and i would like to monitor that voltage by software to give a warning when the time to replace it is reached. I have found no Lo-Bat bit, as known from external...

sk-st by Associate III
  • 1210 Views
  • 1 replies
  • 0 kudos

FSMC 8 bit bus

Posted on September 22, 2014 at 16:21hey all,i am using STM32F4 MCU. trying to connect LCD controller (ILI9342C) using FSMC.i understand that i can use the 8 bit bus.how can i determine which bus to use : D0-D7 or D8-D15Thanx #fsmc

Fast IR camera data tranfer to computer

Posted on September 20, 2014 at 13:12Hello, I am working on projects that takes snapshot from camera, stores it to SRAM via DMA, and when process image by some mathematics, and calculate beam spot on sensor. And sends information to computer, where ...

Understanding FSMC arbitration

Posted on September 22, 2014 at 12:38I want to direct drive a rgb tft display via FSMC/DMA and an external async sram as framebuffer. The cpu is a STM32F103ZC. What happens when CPU writes between transfers to RAM? The transfers would be then: DMA R...

sk-st by Associate III
  • 939 Views
  • 1 replies
  • 0 kudos

Ultrasonic sensor

Posted on September 19, 2014 at 15:02Hello everyone, how can i configure an ultrasonic sensor with timers on stm32f4 ? #interface-anything-to-anything #ultrasonic-sensor

Newbie looking for help with GPIO

Posted on September 01, 2014 at 23:00 I have an STM32F4 Discovery board, which I am relatively new to. I'm trying to figure out how to work with GPIO's, and I haven't been able to find a good tutorial yet, so I'm trying to work it out by looking...

sandtime by Associate II
  • 3798 Views
  • 6 replies
  • 0 kudos

Free real-time operating system on STM32F100RB-Discovery

Posted on September 19, 2014 at 10:26Hi people, I have STM32F100RB-Discovery board. I need a free real-time operating system which I could deploy on that board. I know for FreeRTOS, but following their manual I haven't succeeded to deploy it yet. A...

ing2 by Associate
  • 1561 Views
  • 3 replies
  • 0 kudos

UART4 IRQ Handler not firing

Posted on September 20, 2014 at 11:50With my STM32F4 discovery board I cannot get the UART4_IRQHandler to be triggered on incoming serial data. However the USART2_IRQHandler functions as expected and when the data is ready from the UART4 RX data reg...

andrew23 by Associate II
  • 1833 Views
  • 2 replies
  • 0 kudos