cancel
Showing results for 
Search instead for 
Did you mean: 

problem with stm32f4 discovery SPI2

mohamad_armoon
Associate III
Posted on February 21, 2014 at 01:42

hi guys.

i want to use my stm32f4 spi2 and i wrote some code and i think it should be true,

because i wrote the same code for SPI1 in this board and it works very well,

all i want is to send a data through  mosi and receive that data from miso and show that specific data through usart and serial port in my pc.

pls tell me what is the problem. is my code wrong ??

here is mu code : 

&sharpinclude <stm32f4xx.h>

   

void RCC_configuration()

{

   RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

   RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);

   RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

//    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

   RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

}

void init_GPIO()

{

  GPIO_InitTypeDef GPIO_InitStruct;

  /* configure pins used by SPI1

* PB13 = SCK

* PB14 = MISO

* PB15 = MOSI

*/

  GPIO_InitStruct.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14|GPIO_Pin_15;

  GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; 

  GPIO_Init(GPIOB, &GPIO_InitStruct);

  

  // connect SPI1 pins to SPI alternate function

  GPIO_PinAFConfig(GPIOB, GPIO_PinSource13 , GPIO_AF_SPI2);

  GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2);

  GPIO_PinAFConfig(GPIOB, GPIO_PinSource15 , GPIO_AF_SPI2);

         

}

void init_SPI2()

{

        SPI_InitTypeDef SPI_InitStruct;

        

        SPI_InitStruct.SPI_Direction =SPI_Direction_2Lines_FullDuplex; // set to FullDuplexmode, seperate MOSI and MISO lines

SPI_InitStruct.SPI_Mode = SPI_Mode_Master;      

SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; // one packet of data is 8 bits wide

SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low;        // clock is low when idle

SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;      // data sampled at first edge

SPI_InitStruct.SPI_NSS =SPI_NSS_Soft;

SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; 

SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB; // data is transmitted MSB first

SPI_Init(SPI2, &SPI_InitStruct); 

SPI_Cmd(SPI2, ENABLE); // enable SPI2

}

void init_usart(void){

GPIO_InitTypeDef GPIO_InitStructure;

USART_InitTypeDef USART_InitStructure;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;

GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);

USART_InitStructure.USART_BaudRate = 9600;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Tx;

USART_Init(USART2, &USART_InitStructure);

USART_Cmd(USART2, ENABLE); 

}

   

int main()

{

  RCC_configuration();

  init_GPIO();

  init_SPI2();

  init_usart();

  uint8_t received_val = 50;

  

  while (1)

  {

    SPI_I2S_SendData(SPI2,0x33);

    received_val = SPI_I2S_ReceiveData(SPI2);

 

      USART_SendData(USART2,received_val);

  }

}

#master #stm32f4 #discovery #spi
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on February 21, 2014 at 03:38

RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

So APB1 then.

SPI_I2S_SendData(SPI1,0x33);

received_val = SPI_I2S_ReceiveData(SPI1);

SPI2??

And you should perhaps be attentive to the TXE/RXNE states of the SPI/USART?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mohamad_armoon
Associate III
Posted on February 21, 2014 at 09:35

that's right i fixed it in my code(SPI) but i forgot to fix it in forum. but the problem is exist.

what you mean by  TEX/RXNE state of the SPI/USART??

you know i test exactly the same code for SPI1 then connected PA6 and PA7 together and it worked well. i just changed the GPIO pins and configuration for SPI and connected PB14 to PB15  but it doesn't work. is there any thing that i should do??

waclawek.jan
Super User
Posted on February 21, 2014 at 10:13

Clive pointed it out above:

RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

should be

RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

JW
mohamad_armoon
Associate III
Posted on February 21, 2014 at 10:31

thank you soooooo much guys