STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC on F407 versus F42x/43x

Posted on September 23, 2014 at 13:59Hello, with regard to ADC noise on the F407, AN4547 (F407 -> F42x migration) tells: '' Resolved with new behavior to enhance the accuracy'' However I don't see any description of the new behavior! Can anybody cla...

STM32F4 USB HID: transmit interrupt

Posted on September 16, 2014 at 13:42Hi,The STM USB HID stack generates an interrupt when new data have been received (eg 64 bytes). It is necessary to poll the status (using the USBD_HID_RecReport function), but this is no problem in my application...

koster by Associate III
  • 5203 Views
  • 8 replies
  • 0 kudos

PWR_ClearFlag(PWR_FLAG_SB) not work

Posted on September 23, 2014 at 13:15Hi.I am using the STM32F205ZC and I try to clear the StandBy flag by this command.PWR_ClearFlag(PWR_FLAG_SB). But it doesn't work. I try manual to go to PWR_CR->CSBF and clear there but no help.Only when I active...

Barbie by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

Interference when using SSD1963 and SDRAM over FMC

Posted on September 19, 2014 at 23:43Hi everyone, This is my first post on this community, that i found great, so before everything let me say thank you. I'm currently working on a spare time project which involve some basic PID simulated control/pr...

davide by Associate II
  • 3412 Views
  • 8 replies
  • 0 kudos

STM32F437VI

Posted on September 22, 2014 at 08:05Hi This is a very general question. I am new to cortex M4 processors. I would like to know if I can use a piece of code written in a cortex M4 processor (say STM32F437VI) in any of ST's cortex M0+ or M3 processor...

Instant overrun when enabling via HAL_UART_Receive_IT

Posted on August 07, 2014 at 07:13Hi all,I had an overrun error issue between successive calls to 'HAL_UART_Receive_IT()'.I know what causes the overrun, but shouldn't the following lines be added to HAL_UART_Receive_IT() to clear any pending error ...

uart4 interfacing of stm32f4discoveryboard

Posted on September 22, 2014 at 12:49Hi everyone,I am trying hard to make my uart4 code to working.But I am not getting anything on my hyperterminal.I am using keiluvision4.I have uploadeed th epiece of my code below.Please have a look and suggest m...

Mising startup file

Posted on September 23, 2014 at 00:15Hi All,I have done a search to no avail on this:Using Keil tools and Cube 4.3.1 (STM32F407), generating the project results in missing the startup file - but only at random.The folder ''Application/MDK-ARM'' does...