STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

error in programming

Posted on September 20, 2014 at 11:16hi every onewhen im trying to programm my stm32f103ret6 via jlink in keil v5.11, it shows this error:can any body help me please?WBR #stm32f103 #jlnik

0690X00000602xsQAA.jpg
mhdizgah by Associate II
  • 1869 Views
  • 4 replies
  • 0 kudos

STM32F429 UART7 Rx question

Posted on September 19, 2014 at 13:19Hello friends.I'm trying to communicate with DS18B20 via 1-wire interface.Here is the example of reset function (all pins and clk are set erlier). The problem is that the variable data does not receive UART7 DR v...

baev_al by Associate III
  • 3348 Views
  • 10 replies
  • 0 kudos

stm32f429 I2C clock speed

Posted on September 19, 2014 at 22:58 hello guys, I have a problem with the clock speed of my I2C bus, I want to have 100 hz of frequency but I am not able to reach it. That is my code * @file Touch_Panel/main.c * @author MCD Application Team...

Data structure for data write and Data read

Posted on September 19, 2014 at 22:27 I would like create a variable that contains port and pin information, so I can use the high level name to perform all reads and writes. I am looking for help with the syntax to create a: Structure for...

ebommer by Associate II
  • 2574 Views
  • 2 replies
  • 0 kudos

need to have time separate from main loop_stm32f407

Posted on September 19, 2014 at 15:30hi every body in my program i need to do somethings in specific time , this ''time'' is not equal all the time.for example for doing first job i need to do it 5 sec after a flag become set. and after that i need ...

DMA2 (Can't Configure Seperate Streams for ADC1 and ADC2)

Posted on September 18, 2014 at 17:44I have the STM32F407 Discovery board. I am configuring two streams using DMA and ADC The first stream uses Stream 0 channel 0 of the DMA 2 ie ADC1 which reads the value of ADC chanel 9 1N9 and gets sent to circu...

Puzamoya by Associate II
  • 3174 Views
  • 7 replies
  • 0 kudos

The importance of DMA for ADC

Posted on September 19, 2014 at 10:11Hello,I am wondering what's the utility of using the DMA when getting informations from ADC IP. Thank you.Best regards #adc #dma

anes by Associate
  • 1274 Views
  • 2 replies
  • 0 kudos

Feed Two GPIO From Same Timer?

Posted on September 19, 2014 at 16:25I had been using two different timers based on a PLL to feed two different GPIO pins. It may be creating some timing shifts that my hardware (custom ASICs) don't like. I tried feeding both GPIO from the SAME Time...

jvavra by Associate III
  • 1386 Views
  • 3 replies
  • 0 kudos

STM3210B Not getting detected

Posted on September 10, 2014 at 22:09Hi,I have STM3210B and I am trying to connect it to PC. However, I am unable to connect it. I have installed all the STLink V2 drivers. Besides, I also download STVP tools as well, which installed its drivers.Whe...

shauns87 by Associate II
  • 4139 Views
  • 11 replies
  • 0 kudos

Three PWM signal with variable phase shit and duty cycle

Posted on September 19, 2014 at 12:34 Hello, I want to generate three phase shifted PWM signals whit variable duty cycle and phase shift using SMT32F407VGT.  Is this possible?  I found this post on my.st.com https://my.st.com/public/STe2ecommunit...

sh2 by Associate II
  • 1152 Views
  • 1 replies
  • 0 kudos