STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART: ORE=1, but RXNE=0?

Posted on September 13, 2011 at 09:10Sometimes my code gets lost in usart1 interrupt flood.Registers:CR1: 0x202c (UE, RXNEIE, TE, RE)CR2 = 0, CR3 = 0SR: 0x1d8 (LBD, TXE, TC, IDLE, ORE)I'm not quite getting it how ORE can be set and RXNE not. The onl...

domen23 by Associate II
  • 2997 Views
  • 4 replies
  • 0 kudos

Bug in USART_GetITStatus() re/ USART_IT_ORE?

Posted on June 18, 2014 at 20:24Could someone please confirm the following issue ?, p.706/914 states that: ''ORE: Overrun error (...) An interrupt is generated if RXNEIE=1 or EIE = 1 in the USARTx_CR1 register.'' The hardware indeed appears to work ...

Can't increase USART Baud above 130Kbps?

Posted on September 29, 2014 at 23:16 Hi all, I've been getting familiar with the RCC stuff on the STM32L152 (STMrecently152L-Discovery), but I'm struggling to push the baud rate of my USART transmission beyond 130Kbaud. I've set u...

Queue with uart for Nucleo L053-R8

Posted on September 29, 2014 at 23:44 Hi, I'm a using a Nucleo L053-R8 board and i'm trying to implement a STR system. I'm using CMSIS RTX. And i want to implement a queue in RTX with a peripheral in reception mode(uart) . ...

dauphin by Associate
  • 595 Views
  • 0 replies
  • 0 kudos

Usart send more than one character

Posted on August 17, 2011 at 10:39Hello, I saw that in usart.c there is the function   USART_SendData(USART2, 'a'); but this is for only one character (here 'a'). I want to send more than one character but I can't find how. I think that USART_SendDa...

cyril2399 by Associate II
  • 6352 Views
  • 14 replies
  • 0 kudos

Embedded_GUI_Library Fonts

Posted on December 21, 2012 at 12:32Hello, The GUI lib from ST has few fonts included, where the biggest is 16x24 (GL_ASCII16x24_Table). Does anyone maybe have bigger ? Even it is kinda big, it is still too small for my purpose. Or maybe there is ap...

M0NKA by Senior
  • 2304 Views
  • 4 replies
  • 0 kudos

CYCLONE for STMicro

Posted on September 29, 2014 at 20:21Has anyone used the Cyclone for STMico programmer? Does this programmer only use *.s19 records?

edavis by Associate
  • 875 Views
  • 1 replies
  • 0 kudos

Issue with USART RX buffer and char filter

Posted on September 12, 2014 at 07:21 Hello all, i started a little project with my discovery board, using stm32f407vg and a ublox neo 6m gps. The comunication between the two is done via USART1. At every second the gps sends somewhere at 50...

Bogdan by Senior
  • 3829 Views
  • 7 replies
  • 0 kudos