STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 + SDIO + FatFS

Posted on May 19, 2014 at 15:36Hi all,I've a problem with my STM32F103. I need to use fat filesystem on SD card to read/write/create files.I've connected the SD card to the SDIO interface and 4 wires mode with 47Kohm pull-up on cmd and data pins.I t...

daniele2 by Associate II
  • 10440 Views
  • 23 replies
  • 0 kudos

overlap time generation

Posted on October 01, 2014 at 09:51How can I generate two signals with a specific overlap  time between them?I mean first signal to be square wave 50% duty cycle and the second one square wave inverse of the first one but with overlap time, that is ...

ionutF by Associate III
  • 996 Views
  • 1 replies
  • 0 kudos

STM42F407VG/MB997C I2S3 output silent

Posted on September 30, 2014 at 15:27 Hello, I've been trying to get any life out of the I2S3 output from my STM32 Discovery board, but for some reason I cannot even get a clock signal (CK), as seen with oscilloscope. It also never seems...

flux-ti by Associate II
  • 1665 Views
  • 4 replies
  • 0 kudos

I2S Interfacing with MP45DT02 PDM Mic on STM32F4 Discovery

Posted on September 30, 2014 at 21:29Hello,I've been racking my head trying to make sense of how to correctly configure the I2S Hardware to interface with the MP45DT02 microphone. I've been looking at ST's waverecorder.c for inspiration but I think ...

abarr16 by Associate
  • 758 Views
  • 0 replies
  • 0 kudos

ST-LINK/V2 vs stm32f4discovery?

Posted on September 13, 2014 at 01:46I am having troubles setting up IAR Function Profiler so I wanted to double-check: The grey ''ST-LINK/V2'' device vs the debug interface within discovery board. Are these the same exact thing? At least my Windows...

arro239 by Senior
  • 1335 Views
  • 3 replies
  • 0 kudos

PTP implementation in STM32F437ZGT6

Posted on September 17, 2014 at 09:35Hello. I am working in a R&D Project with the STM32 MCU. I have implemented Ethernet functionality like examples provided by ST. Frame transmission and reception are OK (checked with Wireshark). Now I must add PT...

0690X00000605A5QAI.png
Jose_A by Associate II
  • 2813 Views
  • 4 replies
  • 0 kudos

STM32L0 RCC_CFGR read-only?

Posted on September 30, 2014 at 12:11Hi, I'm using an STM32L051 microcontroller for a low power application. Actually I am working on a state change between low power and normal operating mode. Therefore I am trying to switch the system clock to PLL...

cschumann by Associate II
  • 1204 Views
  • 1 replies
  • 0 kudos

Connection issue

Posted on July 24, 2013 at 09:47Hi,Until yesterday I haven't got any problems to launch my code into flash memory with CooCoxIDE. STLink utility and STMStudio have worked well also.But this morning, I can't do all thius things :C:\CooCox\CoIDE>''C:/...