cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Cube bug - wrong crystal value put in Keil project

rgledhill
Associate II
Posted on March 20, 2014 at 14:26

Hi,

When generating a project for the STM32F4xx, it incorrectly puts 8MHz into the crystal property of the Keil project.  This should be 25MHz as fitted to the board.

Thanks

Richard
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 20, 2014 at 15:19

Does anything actually use that value? The only really critical value in Keil is that of the CPU clock for the Trace/SWV functionality, and the library code which depends on HSE_VALUE being defined correctly.

The DISCO boards use 8 MHz, the EVAL 25 MHz, generally.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..