Touch Sensing Controller STM32L476ZG
Moved from the STM32CubeIDE forum as not related to STM32CubeIDE What is the range of sampling capacitor value in Touch sensing controller?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Moved from the STM32CubeIDE forum as not related to STM32CubeIDE What is the range of sampling capacitor value in Touch sensing controller?
Hello All, I am using the Internal RTC of STM32F767 MCU. The VBAT pin is connected to an External 3.3V Coin Cell Battery At Power ON (Debug window on STM32 Cube IDE), before HAL_INIT when i see the value of RTC BKP1R Register it is 0x5432 as I intend...
Hi Everbody,im trying to setup a SPI com with a DRV8301. im using de STM32G431CBU6. a have read the datasheets mutiple times not saying that i did everything correct but i dont see it anymore. i was hoping that its just a *** mistake and some can pin...
Hi all. I am aware that this topic has been discussed before here: https://community.st.com/t5/stm32-mcus-products/debugger-hangs-at-scb-enabledcache/td-p/640648 and here: https://community.st.com/t5/stm32-mcus/dma-is-not-working-on-stm32h7-devices/...
The STM32H7(4/5) documentation states that two of the ADCs on board can be used in dual ADC mode, so that their 16bit samples are read into the upper- and lower halfwords of a single 32bit register (ADCx_CDR), from where a single DMA can read them in...
I am facing an issue connecting the STM32F4 NUCLEO-F429ZI board to an HMI screen that uses RS232 and RS485 communication standards. The HMI can communicate successfully with my computer, but the STM32 board cannot communicate with the computer exce...
Hello ST Forum,We are using an STM32H750I in a current project. This STM communicates via the USART1 with another STM32H750V at a baud rate of 512kBaud. The clock of the STM32H7 runs via an 8MHz HSE (external quartz) at 480MHz. The clock of the USART...
Hello evryone:at the first it is may firt project with STM32, and don't have any experince with this MCU.I have a problem, when I read (with HAL_ADC_GetValue(&hadc1)) the multi channel ADC value in interrupt mode the value is always the same. I have ...
Hi,I am working on a project for a STM32G473CE, that is already working with the v1.0.0 of the OpenBootloader with FDCAN in order to flash the MCU.I want to upgrade the OpenBL to the latest version (v6.0.1 : https://github.com/STMicroelectronics/stm3...
I checked the datasheet and there is a memory map of 521Kbyte.But I use the stm32h523VCT6 chip.This chip has 256Kbyte of memory.Can't a chip with 256Kbyte of memory use bankswap?If it can, can you tell me the memory address?