Problem ping in stm32f429zi
Hello St's,I got ping problem, could you please help to figure out this problem. Thanks
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hello St's,I got ping problem, could you please help to figure out this problem. Thanks
Hi Why do STM32 microcontrollers that support MIPI not have speeds of 480 MHz or higher?
Hi,I'm thinking what is the right way to clear HRTIM interrupt status register (HRTIM_ISR) bits?In the description of the HRTIM_ISR register STM32G4 reference manual (RM0440 Rev 8 page 1041) says: This bit is set by hardware when fault 1 event occurs...
Hello to all I would like to use the eMMC that comes with my board (STM32H745I-Disco) but I'm a bit lost. where can I look for examples?I would like to keep a simple structure to start with and then read it. Something like: typedef struct { char ...
Hello,I'm trying to generate a custom PWM output signal with the F103V8TxLQFP100. I took inspiration from here: Custom Signal generation using PWM and DMA - STMicroelectronics CommunityThe basic code looks like this:...uint8_t tempBuffer[10];tempBuff...
I've been looking at the information on the flash organization in the Reference manual RM0456 for STM32U5. In particular I'm trying to understand how the DUALBANK flag works on this family.In section 7.3.1, there is this table for STM32U5G with 4MB ...
I am not able to activate LWIP middleware for M7 core on any dualcore STM32. (I am able to do it on single-core devices and already have LWIP working on H743 Nucleo)Steps I have done (exactly in this order):- create a new project for STM32H757IITx i...
I have been working on a self learning project with STM32G431 controller. I am having trouble switching on the PLL to get 170MHz.When I use the CubeIDE, I get the 170MHz clock. Given below is my code on how I am trying to Initialize the PLL//PLL sett...
I connected this resonator https://jlcpcb.com/parts/componentSearch?searchTxt=C341522 And the code runs. - however - USB fails to enumerate.If I upload the same code to a BluePill board, the code runs *and* the USB works.I suspect it being due to s...
Hello Community, I am planning to use I2C operating at 1kHz maximum on STM32G4 & STM32G0 series for measuring temperature from Digital Temperature sensors placed at 2m distance from the main board in an industrial environment using CAT6 (STP) Cables ...