User Activity

Hello everyone, I'm using the STM32CubeIDE , then I would like to ask about the ADC configuration for the STM32F429 board. Currently, I want to distinguish a sine wave input ranging from 10kHz to 3MHz, the ADC parameters are set as follows:(1) APB 1 ...
Hi everyone,I'm encountering an issue with generating a 1 MHz sine wave using the DAC, TIM, and DMA for DDS. I'm utilizing a wave table to generate the sine wave.Currently, I have the HCLK and APB2 clocks both set to 180 MHz, and I'm using TIM8 as th...
Hi, I'm having some problems with the STM32F429 DAC testing. I have two boards of the same type. On board 1, the Digital Storage Oscilloscope shows that the sine wave voltage ranges from 2.08V to 2.94V. However, on board 2, with the same program and ...
Kudos given to