STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to change target device in STM32CubeMX

Posted on December 13, 2014 at 00:19How do I change the target device in STM32CubeMX?  Do I need to recreate the entire project and copy over the user sections?  or is there a simple way to do it?Right now, I only want to change from STM32F302R8T6 t...

caleb by Associate III
  • 1841 Views
  • 2 replies
  • 0 kudos

Loosing scope in global variables

Posted on January 08, 2015 at 14:22Hello!I'm using STM32 CubeMX 4.3.1 generating code in Keil. I experienced extrange behavior with Global variables. It seems as if at some point within a function a local variable loses its contents...But debugging ...

edmunoz by Associate II
  • 1420 Views
  • 2 replies
  • 0 kudos

STM32 software reset

Posted on January 08, 2015 at 13:46Hello, I want to know what happend when I do a software reset exactlly. I use the function NVIC_SystemReset that set the SYSRESETREQ bit. In the documentation I found:The SYSRESETREQ bit in Cortex™-M4F Application ...

yohann by Associate II
  • 2186 Views
  • 2 replies
  • 0 kudos

Taking microsecond timer without interrupt

Posted on January 08, 2015 at 13:29Hello I'm looking for a solution to get the time between to input signals in microsecond resolution. But I do not want to use an interrupt counting up all microseconds. Is there a convenient solution / method? #...

oli by Associate II
  • 1022 Views
  • 2 replies
  • 0 kudos

[QUESTION] About machine cycle of STM32 and STM8

Posted on January 06, 2015 at 10:30Hello, I want to ask you a question. How many crystal cycles make up a machine cycle are in STM32 and STM8? For example, in 8051, 12 crystal cycles make up 1 machine cycle. Thank you!

ADC with DMA arrest on STM32F4

Posted on December 09, 2014 at 14:19Dear All,My board is 429I-DISCO. I tried to code a continuous A/D conversion via DMA on FreeRTOS. At first A/D conversion shortly after power-up was starting nomally by ADC_SoftwareStartConv(ADC3). On the rest of ...

yoshi by Associate II
  • 3789 Views
  • 11 replies
  • 0 kudos

ARM Accredited MCU Enginner

Posted on January 08, 2015 at 07:09A Question and Answer Book ''ARM Accredited MCU Enginner''http://www.amazon.com/dp/B00R9BYWWA #arm-cortex-accredited-mcu-aame

Multiple ST-link Debuggers

Posted on December 23, 2014 at 12:59Hi, I'm debuging a network application running across multiple Nucleo boards with multiple instances of the Keil IDE. Every time a target leaves the debugger the ST-Link connection is lost and reconnection becomes...

occam by Associate II
  • 2602 Views
  • 3 replies
  • 0 kudos

STM32F429 - cannot view external memory in Eclipse memory pane.

Posted on October 24, 2014 at 21:19I have been utilizing Eclipse IDE using GNU tool chain to develop and debug my STM32F429 based project.The target platform has an external SDRAM memory which configured and managed by the MCU's FMC unit. Even thoug...

kurt1 by Associate II
  • 1432 Views
  • 2 replies
  • 0 kudos