STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 100 I2C peripheral not sending address

Posted on January 07, 2015 at 12:51 I am trying to use the I2C peripheral on the STM32 I am finding that about half the time the address isn't being sent. What happens is that the data line is going low (start condition is set) the clock line go...

SPI clock phase setting

Posted on January 06, 2015 at 09:26I am using STM32L152 part to talk to a digital accelerometer using SPI. The SPI signal timing diagram for the accelerometer is illustrated in the attached figure. Looking at the diagram, it is clear that the spi cl...

bnp979 by Associate III
  • 6484 Views
  • 6 replies
  • 0 kudos

How to declare a big array in external SDRAM?

Posted on January 06, 2015 at 14:03I use STM429 and 128Mb SDRAM and want to decare a big array in keil. How to declare it? How to let keil linker know the array is in external RAM? I defines uint8_t temp[1024*1024], but linker error L6406E: no space...

ray by Associate II
  • 2104 Views
  • 3 replies
  • 0 kudos

Jumpers for STM324x9I-EVAL I/O connectors?

Posted on January 06, 2015 at 15:18These are the 0.05'' (1.27mm) pitch connectors CN6, CN7, CN11 and CN12. The jumpers I normally use on 0.10'' pitch headers are too big to fit. I've done some web searching and not found any jumpers that size. What ...

hbarta2 by Associate III
  • 1333 Views
  • 2 replies
  • 0 kudos

Unstable working of I2S on STM32

Posted on August 08, 2013 at 21:17I faced a critical problem of i2s of STM32.I'm developing a simple system for i2s level meter.MCU - STM32F103RCT6 with external X-tal(12MHz), 72MHz of running clock Inpit Audio - 48KHz, 16bits, stereo i2s digital au...

cubefilm by Associate
  • 2270 Views
  • 4 replies
  • 0 kudos

Vector table relocation

Posted on January 05, 2015 at 17:44I have relocated the Vector Interrupt Table as follows         *((volatile uint32_t *)0xE000ED08) = 0xFFFFFF00 & 0x08004400;                 // jump to bootloader         pVector = GetBootStartEntry();         asm ...

ivesely by Associate II
  • 2782 Views
  • 4 replies
  • 0 kudos

Code generation tool for Std. Peripheral library?

Posted on December 20, 2014 at 16:41Hi everyone,I was wondering if there is a tool like STM32CubeMX to generate initialization code with the standard peripheral library.The Cube is too new and still needs to mature but i do like the STM32CubeMX tool...