STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Respiration Rate using stm32f429i discovery kit

Posted on February 11, 2015 at 11:27I am just working on vital sign monitor project. I have a stm32f429i discovery kit. We are using capacitive sensor for respiratory signals, its very weak signals. Sensor output will be fed to adc of microcontrolle...

lokesh by Associate II
  • 1103 Views
  • 1 replies
  • 0 kudos

DFU Bootloader

Posted on June 17, 2014 at 10:53Hi folks,I have ST's Flash Loader Demo application for programming via a UART and was wondering if anyone knows if there's an equivalent for programming via USB. I want to use the DFU bootloader so I can program witho...

Firmware update via ethernet

Posted on February 04, 2015 at 11:08Hai all,   I am sending GPIO toggle application via ethernet to STM32F407.My application total length is 2920(.hex file).But in controller side i am getting 1460 data only.In controller i am receiving data like,  ...

STM32F4 problem with Encoder Interactive od TIM HAL

Posted on February 09, 2015 at 15:24Hello,I'm learing to use STM32Cube and HAL.Then I tried to set TIM encoder mode,but it can't work.This is my code of initialization and functionCan someone tell me ,what mistake I made or what important step I mis...

azura817 by Associate
  • 1037 Views
  • 2 replies
  • 0 kudos

Power Line Communication(PLC) on STM32F4

Posted on February 11, 2015 at 01:27HelloI have another work for transferring/receiving data using PLC(Power Line Communication)GPIOA port 12 is for PLC port.so I have looked for many of example and tutorial for 2days but there are no exist.....so i...

dukesong by Associate II
  • 1303 Views
  • 1 replies
  • 0 kudos

STM32F4 receive DMA timeout

Posted on February 09, 2015 at 17:59Hello,I have to realize receive DMA timeout for a serial interface. I found the application note AN3109 which describes a mechanism to realize a DMA timeout for the STM32F10x microcontroller. Does this application...

STM32F303x - Hardware Resets

Posted on February 09, 2015 at 15:51What is the usual procedure for power-on reset for other chips besides the MCU? Is there a reset_out signal or method coming from the MCU that is recommended? Or is there a method for resetting all chips in a syst...

gbigden by Associate III
  • 1924 Views
  • 6 replies
  • 0 kudos

Semihosting in Eclipse or retargeting printf

Posted on June 03, 2014 at 09:43Hi,I am trying to debug some very simple code for STM32F0Discovery using Eclipse, ARM arm-none-eabi-gdb compiler and OpenOCD debuger.I could build and debug my cods and now I am trying to use printf to see some variab...

Rise time of SPI Signal

Posted on February 10, 2015 at 10:50Hi I am using STM32F103RBT6 @72MHZ I use SPI with DMA to stream data from memory to GPIO SPI Prescaler is 4 GPIO is configured as output push-pull and speed 50MHz The problem is that the data output rise and fal...

hossam by Associate II
  • 1565 Views
  • 1 replies
  • 0 kudos

STM32f2xx SWD programmer problem

Posted on February 09, 2015 at 16:34 Hi at all,I would try to program a custom made board with STM32f205RCT7 micro onboard via SWD .I got an SWD connector with vdd,gnd,swdio,swclk,nrst.No pull up or pull down on swdio pin , 10k ohm pull up on nrst a...

andreima by Associate
  • 1418 Views
  • 3 replies
  • 0 kudos