cancel
Showing results for 
Search instead for 
Did you mean: 

DMA problems on SDIO from SRAM at 0x60040094

subscriptions
Associate II
Posted on July 17, 2014 at 09:49

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
waclawek.jan
Super User
Posted on July 17, 2014 at 10:57

> 

| ((0x01 << 23) & DMA_SxCR_MBURST) //4 beat memory burst 
 IMO, FSMC does not support read bursts.
 JW

subscriptions
Associate II
Posted on July 17, 2014 at 14:33

I thought that might be the problem, so tried to do it with a single transfer, but that doesn't work either. Here's the modified code for configuring the DMA:

//Set the DMA CR 
tempreg = DMA_Channel_4 //Select Channel 4 
| DMA_MemoryBurst_Single 
| DMA_PeripheralBurst_Single 
| DMA_Priority_VeryHigh //Priority is very_high 
| DMA_MemoryDataSize_Word //Memory data size is 32bit (word) 
| DMA_PeripheralDataSize_Word //Peripheral data size is 32bit (word) 
| DMA_MemoryInc_Enable //Enable Memory Increment 
| DMA_PeripheralInc_Disable //Disable Peripheral Increment 
| DMA_Mode_Normal //Disable Circular mode 
| ((dir == WRITE_TO_CARD) ? DMA_DIR_MemoryToPeripheral : DMA_DIR_PeripheralToMemory) 
| DMA_FlowCtrl_Peripheral; //Peripheral controls the flow control. (The DMA tranfer ends when the data issues end of transfer signal regardless of ndtr value) 
//Bit [4..1] is for interupt mask. I don't use interrupts here 
//Bit 0 is EN. I will set it after I set the FIFO CR. (FIFO CR cannot be modified when EN=1) 
DMA2_Stream3->CR = tempreg; 
//Set the FIFO CR 
tempreg = DMA_FIFOMode_Disable; //Fifo is disabled (Direct mode is Enabled); 
DMA2_Stream3->FCR = tempreg; 
#endif 
//Enable the DMA (When it is enabled, it starts to respond dma requests) 
DMA2_Stream3->CR |= DMA_SxCR_EN; 

waclawek.jan
Super User
Posted on July 17, 2014 at 14:56

NDTR? LISR?

JW
subscriptions
Associate II
Posted on July 17, 2014 at 16:20

LISR: 0x400000         (FEIF3)

NDTR: 65534             (I'm writing to SDIO, letting the peripheral control flow)

DMA2_Stream3->CR 0x8035461

francescatodiego
Associate II
Posted on July 18, 2014 at 06:22

tries to separate

the problem

Enable

the

DMA

and stop the code execution before 

the

SDIO block

write command

if

the configuration of the

DMA

is correct

you have to see

that the FS field

in the

DMA_SxFCR

register

changes from

0x04

(

FIFO

empty

) to

0x05

(

FIFO

full)

It means that the

DMA

transfer

has

started

ok

and wait

for

SDIO

peripheral

.

I guess the

firmware

checks

the status of the

SD card before

writing the block

and

configure

the block size

before start write.