cancel
Showing results for 
Search instead for 
Did you mean: 

Connect +5v to Ground

Linda
Associate II
Posted on July 20, 2014 at 16:30

I made a mistake by Connecting,  +5v to Ground, now the stm32f429i-discovery doesnot work anymore, only the LED4(PG14) flash.

How to fix it?

Thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on July 20, 2014 at 16:44

Identify the part or parts damaged and replace them. Review the schematic to identify potentially damaged parts, and test the voltages and signals on key pins.

If this fails, replace the board.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Mark Edwards
Associate II
Posted on July 20, 2014 at 23:51

Where was the 5V supplied from? Is it stable (can you check with a meter)? As long as it was only the 5V the main components are all the other side of the regulator (3V) so they should be OK. If you were using the USB to supply it D2 may be damaged and not passing enough current for the board to start up which may explain the LED flashing.

You could try feeding 5V directly onto the board using the 5V pins on the top of P1 and 0V to the bottom pins.

Linda
Associate II
Posted on July 21, 2014 at 02:42

Dear Tede,

I connected the P1(+5v) to the ground by mistake.

Any idea?

Thanks