STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo L152RE: Flash page erase issue

Posted on March 07, 2015 at 13:04 Hi, I'm trying to write and erase data into/from internal Flash memory (range 0x0800000 - 0x0807FFFF) of STM32 L152RE. I'm only accessing the last page of Flash ( 0x0807FF00 - 0x0807FFFF) and then writing the ...

hunarame by Associate
  • 780 Views
  • 0 replies
  • 0 kudos

CMOS Schematics+DCMI+STM32F4xx

Posted on March 07, 2015 at 04:28Hi guys,I need some help understanding a schematic of a cmos image sensor module we are going to purchase due time. The issue is that we have been testing out with a 8bit DCMI using a stm32f429 for previous modules b...

0690X000006030hQAA.jpg 0690X000006030mQAA.jpg

2 udp server with stm32f429 broblem

Posted on March 07, 2015 at 02:57hii used two stm32f429 eval board's as udp server that connected to one pc client and use STM32Cube_FW_F4_V1.3.0(LwIP_UDP_Echo_Server) codepc(as client)<------>(ethernet hub switch)|<----->server-1(stm32f429 as udp s...

ADC

Posted on March 05, 2015 at 20:10I need simple stand alone test program which will convert more than one channel when needed. My requirements NOT to use Standard peripheral library, do everything manually, No IRQ nor DMA. The goal is to understand w...

Clipped sine input for HSE clock input on STM32F303?

Posted on March 06, 2015 at 10:52I am using a STM32F303 and need a very high stability clock ie around 1ppm over temperature. One of the modules I am looking at outputs what is described as ''clipped sine''. Can this drive the oscillator input on th...

gbigden by Associate III
  • 861 Views
  • 1 replies
  • 0 kudos

SWD clock restrictions

Posted on March 06, 2015 at 11:33Hello, the STM32 datasheets do not mention any restictions on SWD or JTAG frequency. Some ''internet knowledge'' tells that older ARM cores had a HCLK/6 limitation on SWD/JTAG clock frequency. Has anybody hard facts ...

stm32f407vgt temperature

Posted on March 06, 2015 at 10:39hi every body.recently i designed a board using stm32f4vgt6 , before that i tried my code on stm32f4 discovery board,when i solder micro entirely , and deploy my code on it , micro becomes more warmer than discovery'...

Standard peripheral library for newer STM32 chips.

Posted on February 18, 2015 at 14:44Hi,I don't want to migrate from the standard peripheral library to the STM32cube hal library platform. So I would like to know if will be possible to use the standard peripheral library for newer STM32 chips like ...

Asantos by Senior
  • 815 Views
  • 2 replies
  • 0 kudos

STM32F446 Quad SPI pinout

Posted on January 22, 2015 at 12:35Hi,   I would like to know what is the difference between the pins QUADSPI_BK2_IO3(PE10) and QUADSPI_BK1_IO3 (PA1)?   There are only one quadspi interface on the STM32F446, why BK1 and BK2?       Can I use the pins...

Asantos by Senior
  • 1007 Views
  • 1 replies
  • 0 kudos