User Activity

Posted on July 21, 2014 at 19:34Hi ,1. How Can i Find which version of freeRTOS the STM32CubeMX add to the project ?2. I don't Know if this the right place to ask , but does freeRTOS fully support     CMSIS-RTOS API ?  Thanks .
Posted on July 19, 2014 at 22:33hi ,i am currently evaluating STM32CubeMX for STM32F4 , great tool for getting started on New MCU.I have few question : 1.How can i define User Code block ? so when i make changes to existing project    the STM32CubeM...
Posted on May 26, 2014 at 23:23What is the recommended way to mange simultaneous I�C and RF data transfers with M24SR IC and 2 Host MCU & NFC Phone?I have implemented mechanism with time Slice , so that each Host has time window to communicate with ...
Posted on February 17, 2014 at 09:54hi , 1.what is the page size in M24SR-16  ?  in the datasheet its declared  that    write time for page in I2C = 5ms , write time for up to 264 bytes =150ms 2.Is it normal after writing 5 bytes to the  M24SR , i a...
Posted on February 09, 2014 at 09:26hi , i having a problem with the deselect command , when i want to open and close Session on the I2C interface , the S(DES)  command doesnt close the session (by looking at the GPO) , only by turning ON/OFF the VC...