STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32H73** sleep mode

Hi, My test board can enter sleep mode OK, but doesn't wake up when PC13 goes high: (never reach __enable_irq())  void Sleep() { __disable_irq(); SysTick->CTRL = 0; // Enable WKUP4 (PC13) PWR->WKUPEPR = PWR_WKUPEPR_WKUPEN4; // Enable WKUP4 PWR->WKU...

harareyd by Associate
  • 1478 Views
  • 3 replies
  • 0 kudos

change of dead band issue in PWM

Hi,i was trying to change dead time from (244 value to 100) for every 10ms in a loop. But its not updating , the set dead time is 244 in the PWM waveform. Though my dead band register ( DTG) is updating  at every 10ms. I am updating TIM1->DTR2  if(en...

Sushmita by Associate II
  • 949 Views
  • 1 replies
  • 0 kudos

, ETH[FIN, ACK] and HTTP GET retransmissions

Good morning. I'm running an STM32F767Zi on a custom board, LwIP 2.1.2, no OS. The device acts as a HTTP server. I've got an issue where I get GET requests and [FIN, ACK] packets retransmitted by the web browser.192.168.5.106 - Client192.168.5.196 - ...

Screenshot 2024-10-21 092806.png Screenshot 2024-10-21 150452.png
pelgrimo by Associate II
  • 1339 Views
  • 1 replies
  • 0 kudos

STM32U LPTIM Autonomous Mode

I am using the LPTIM3 with LSEAn external input is used to trigger a capture.The STM32U575  spends most of the time in STOP MODE 2.To keep the LSE active in the LPTIM use the following instruction:_HAL_RCC_LPTIM3_CLKAM_ENABLE(); // SET_BIT(RCC->SRDAM...

dhs by Senior
  • 2231 Views
  • 1 replies
  • 0 kudos

Power consumption of my HW

good morning,I am actually working on my STM32G431KB, I will use the power consumption tool of STM32cube once my code is complete but I would like to know if for now my calculations are correct.I want to use my board to power up 11 different sensor  ...

Jad_0-1732802079947.png Jad_1-1732802117275.png Jad_2-1732802279947.png Jad_3-1732802365385.png
Jad by Senior
  • 1386 Views
  • 2 replies
  • 0 kudos

Resolved! Boot Issue with CM4 - STM32H745ZIT6

Hello Team,We have a custom STM32H745 board designed and We are able to get the IC up and running on cube programmer and even set option bytes. The board is designed with Nucleo-H745ZI-Q schematics and we have verified everything on hardware end.When...