STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA request queue

Posted on April 09, 2015 at 06:10Hi all,I am working on an STM32F0 project in which I am triggering a DMA transfer using peripheral events such as an input capture. Looking over the docs it seems a little vague as to the behaviour of the DMA control...

luke2 by Associate II
  • 1921 Views
  • 2 replies
  • 0 kudos

STM32F4-DIscovery FAT example wrong

Posted on April 07, 2015 at 12:52In example:if(f_open(&MyFile, ''STM32.TXT'', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) Keil output: error:  &sharp167: argument of type ''char *'' is incompatible with parameter of type ''const TCHAR *''        if(f_ope...

chief by Associate II
  • 2414 Views
  • 5 replies
  • 0 kudos

About how to clear Pending Register

Posted on April 08, 2015 at 09:19Hello. I'm struggling with clearing pending register. I'm trying to clear the register in EXTI0 handler, but it looks like my program doesn't work. I'm using HAL driver, HAL_GPIO_EXTI_CLEAR_FLAG like below coding; HA...

Stm32f051 adc for multiple channels

Posted on April 07, 2015 at 09:14 Hello everyone, I have problem with the ad conversion into the stm32f051 microcontroller. My Destination is: AD-convert for multiple channels PC0, PC1, PC2, PC3, PB0 und PB1 My Problem: ...

STM32F373 SDADC common mode rejection ratio question

Posted on April 08, 2015 at 21:28Hello,I am interested in using the sigma-delta ADC on the STM32F373 microcontroller.  I would like to use it in differential mode to measure the output of a load cell bridge - but I have not been able to find any inf...

FATFS STM32F4-Discovery

Posted on April 08, 2015 at 15:40Hi,I am trying to do a memory stick reading in the STM32F4-Discovery board.In order to test it, I am running the application example located in the following path:STM32Cube\Repository\STM32Cube_FW_F4_V1.5.0\Projects\...

lucas23 by Associate II
  • 1902 Views
  • 3 replies
  • 0 kudos

STM32L151 failure accessing FLASH and EEPROM

Posted on April 08, 2015 at 17:04Hi, I am using the micro STM32L151 and I found that after programming the micro some of the micro have problems accesing FLASH and EEPROM.I can not program the micros again because it is not possible to read the FLAS...

ecatala by Associate II
  • 2042 Views
  • 3 replies
  • 0 kudos

STM32 RTOS ERR

Posted on April 07, 2015 at 17:31The original post was too long to process during our migration. Please click on the attachment to read the original post.

herrusw by Associate II
  • 2562 Views
  • 4 replies
  • 0 kudos

ADC in Dual Mode Simultaneously

Posted on July 22, 2013 at 15:27Hi everyones,I am stuying the example from STM32 libraries (ADC_DualModeRegulSimu). I understand how the whole program works but I need some information and I have few questions about this code confronting to my proje...