STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f429 discovery only run at download and debug mode

Posted on April 19, 2015 at 23:45Hello, I'm using IAR and I configured stm32f429 discovery board by STCubeMX and its libraies. It seems to work fine when I run my code with Download and Debug mode. But when I exit debug mode the board stop running ...

Max heap size and allocating memory

Posted on April 24, 2015 at 19:12Hi!I have STM32F407VET6 MCU with 192kB RAM. I need allocate 150kB for storing image after processing data. However I can't allocate such big array. I though I should increase heap size, but I can't increase it more t...

wojdembi by Associate
  • 2766 Views
  • 3 replies
  • 0 kudos

UART receive interrupt

Posted on April 22, 2015 at 19:02I have a board using an STM32F105.  There is a GPS connected to UART4.  I've been trying to get the RXNE interrupt working for a couple of days now, but I must be missing something. The UART seems to be enabled, as I...

Modify the start address 0x800 0000

Posted on June 26, 2012 at 16:26Hi,My microcontroller is a STM32F103CB.I followed the AN2557 to do an IAP in my software. Everything works fine but now I would like to do something like a dual bank features.I can flash two firmwares at two different...

eancelin by Associate II
  • 15325 Views
  • 28 replies
  • 0 kudos

Handling ADC with DMA

Posted on April 24, 2015 at 07:13Hi, I would like to ask how to sample adc values (potentiometer) using DMA interrupt? #adc #dma #stm32f3discovery

kahseng05 by Associate II
  • 1075 Views
  • 1 replies
  • 0 kudos

Question about systick_handler

Posted on April 24, 2015 at 17:35Hi,I am doing development on an STM32F429 using CMSIS-RTOS/RTX.  I am getting the following linker error:.\output\LmMain.axf: Error: L6200E: Symbol SysTick_Handler multiply defined (by hal_cm3.o and stm32f4xx_it.o).H...

Catch 22 on reset with stm32f303 using ST-Link

Posted on April 24, 2015 at 15:14The problem is simple. I uploaded a buggy program using ST-Link to a stm32f303 prototype board. The bug was that the routine that kicks the watchdog in the power supervisor does not work. Therefore it keeps resetting...

gbigden by Associate III
  • 1397 Views
  • 3 replies
  • 0 kudos

Cannot view any discussions

Posted on April 23, 2015 at 14:55All I get is an error page that says:''An unexpected error has occurred./public/STe2ecommunities/mcu/_layouts/spcontnt.aspx?&url=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder%3d%252fpublic%2...

gbigden by Associate III
  • 1459 Views
  • 4 replies
  • 0 kudos

Simple reset h/w question

Posted on April 24, 2015 at 12:48On the Discovery F3 board I see in the schematics that the hardware reset (NRST) is a switch to ground in parallel with a 100n capacitor. This appears to double up as a power-on reset. Is this correct and is it suffi...

gbigden by Associate III
  • 2111 Views
  • 6 replies
  • 0 kudos