User Activity

Posted on December 13, 2014 at 17:41Hello everybody,I am developing a system in wich a STM32F103 microcontroller has to communicate with a master receiver external device. I have to configure the STM32 as a I2C slave transmitter in order to send dat...
Posted on November 25, 2014 at 23:48Hi everybody, these days I'm starting a project based on STM32F103RE uC for which I have to use the CAN bus pheripheral to transmit and receive messages.I have no previous experience with CAN pheripheral on STM32 ...
Posted on October 10, 2014 at 16:15Hello everybody,I am searching for a CAN transceiver for STM32F103 based board I am developing.I was interested in the AMIS-30633 transceiver, it is automotive certified and it is ISO 11898 compliant. The STM32 CAN...
Posted on September 16, 2014 at 17:38Hi everybody,I'm working about the creation of an automotive dashboard and I'm going to use a STM32 microcontroller, in particular a STM32F103.I'd like to have some suggestions about the LCD display choice, here ...
Posted on March 03, 2014 at 17:40Hello everybody. I am developing some test firmwares on a STM32F103 based board. After some working programs using the sleep mode, now I need to do some experience with the much more powerful standby mode. I need to ...