STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Compilation error with c++11 dialect

Posted on June 09, 2015 at 15:44Hi, I would like to use C++ 11 dialect with ac6 tools suite. But I get a compilation error that I'm not able to handle. Code : register char* stack_ptr asm(''sp''); Error : error: expected '=', ',', ';', 'asm' or '...

JulienD by Senior
  • 1431 Views
  • 5 replies
  • 0 kudos

READ from OTP

Posted on June 12, 2015 at 09:48Hejcan anyone tell me how to read from OTP. If possible put some sample code.Thank you ..

arunl4g by Associate II
  • 2186 Views
  • 5 replies
  • 0 kudos

STM32F4DISCOVERY - compatible IDEs (free)

Posted on June 14, 2015 at 20:57Noob here.  Have done with with AVR 8-bit and want to move-up and try the STM32F4.  Is there a free or inexpensive IDE available that is not code-limited?  Thanks.

nobody102 by Associate II
  • 1174 Views
  • 2 replies
  • 0 kudos

ST-LINK CLI

Posted on May 30, 2015 at 02:47Hello, Is somebody could say me if there is some issue with ST-Link CLI to write bin file? Command doesn't take the address parameter 0x08000000 and try always to write at 0x00000000. Please see my screenshot below. Th...

0690X00000605gQQAQ.png

FSMC, getting confused...

Posted on June 12, 2015 at 19:08So I have an STM32 F103ZET. We use a UC1701 controller to drive a small LCD. It's attached to FSMC Bank1, 2nd section, using an 8bit wide bus. I've been able to write control data using the address 0x64000000 to direc...

GregMusic by Associate II
  • 2502 Views
  • 5 replies
  • 0 kudos

Coherent dual channel (multimode) sampling on STM32F4

Posted on June 12, 2015 at 12:02Hi All,  I am learning how the  ADCs  modes are working on the ST32F4 MCU (using Olimex board). I got operational  ADCs (running independently)  in  a single a and continuous mode. The next step is to get a coherent s...

darek by Associate
  • 1284 Views
  • 2 replies
  • 0 kudos

STM32F051 -> ADC1 -> sometimes no value returned....

Posted on June 07, 2015 at 11:43 Dear community, I investigated the ADC_BasicExample given in the STM32F0xx_StdPeriph_Lib_V1.5.0 Database. I did a few changes since I want to analyze the converted value with the PC via UART. However I noticed ...

jogerh by Associate II
  • 2885 Views
  • 7 replies
  • 0 kudos