STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Replacement for NVIC_SetVectorTable ?

Posted on June 16, 2015 at 01:35 In the latest HAL on the F1 (and F4) (http://www.st.com/st-web-ui/static/active/cn/resource/technical/document/user_manual/DM00154pdf ) Doesnt seem to contain NVIC_SetVectorTable(NVIC_VectTab_FLASH, USER_PROG_O...

STM32F405 Won't Oscillate ?!?

Posted on June 15, 2015 at 23:33Hello: This problem has me totally dumbfounded. Please see the attached image and screen shot of schematic. An absolutely simple circuit, yet it does not want to oscillate. This is the second board (different PCB, dif...

ADC Common Status Register

Posted on June 12, 2015 at 21:59The STM32F429 has three ADCs: ADC1, ADC2, and ADC3. They all have a status register, which has an EOC bit to indicate conversion complete.There's also a common status register (ADC_CSR) shared by all three ADCs that c...

jerry2 by Senior
  • 3057 Views
  • 7 replies
  • 0 kudos

[solved] STM32L151UC: SPI3 problem - no activity on pins

Posted on June 15, 2015 at 14:20Hello, I am trying to configure the SPI3 port of an STM32L151UC micro controller. I have tried several things but I see no output on the related pins. When using gpios instead of the AF of the SPI peripheral, I can ...

bxCAN Master vs Slave

Posted on June 12, 2015 at 14:20I would like to connect to my car's CAN network but I'm a little confused as there are two CAN interfaces in STM32F407 - CAN1 (Master, PB8 and PB9) and CAN2 (Slave, PB5 and PB6). Why do we need two interfaces? Can you...

usb host MSC send&receiveData

Posted on June 01, 2015 at 11:27 I made a project with stm32cude mx for stm32f401 discovery, discovery board is usb msc host, send a command to devide (usb msc device) then receive data form device my project connected and saw all infomati...

Khoa Tran by Associate II
  • 1214 Views
  • 1 replies
  • 0 kudos

Problem caused by NRST pin to perform system reset

Posted on June 15, 2015 at 10:26Hi,I am using STM32F405.The NRST pin is connected to Vdd through a 100k pull-up resistor and to GND with a 0.1uF capacitor, just follows the design of STM32F4-Discovery. The NRST pin is also connected to GND with a 2-...

How to specify external interrupt rather than event

Posted on June 15, 2015 at 10:41 Hi, Using the cube 4.8.0 I configured PA2 to be GPIO_EXTI2 because I want an interrupt generated when the signal connected to that pin goes low but the code that gets generated for me looks like this:   /*Configure G...

markb by Associate II
  • 1565 Views
  • 2 replies
  • 0 kudos