Skip to main content
brent23
Visitor II
December 11, 2014
Question

STM32F103 Standby Mode Resets Processor Immediately

  • December 11, 2014
  • 0 replies
  • 575 views
Posted on December 11, 2014 at 10:04

Hello,

I'm trying to use the STANDBY low power mode on the STM32F103. I have verified that the User Option Bits are set such that IWDG=1, NoReset_STOP=1, NoReset_STBY=1. Therefore the processor should not reset when entering either STOP mode or STANDBY mode.

The following code seems to reset the processor even though NoReset_STBY=1:

void bl_mode_standby(void)

{

    __disable_irq();

    PWR->CR |=  PWR_CR_CWUF; // In case the pin was high already

    EXTI->PR = 0x007FFFFF;  // Clear any pending EXTI interrupts

    PWR_WakeUpPinCmd(ENABLE);   /* Enable wake from WKUP pin*/

    PWR_EnterSTANDBYMode();

}

When I check the reason for the reset RCC->CSR = 0x0c00_0000, meaning that it was a Power On Reset & NRST Pin. One thing to note on this HW design, the NRST is not connected (NC), but should have an internal pull-up. Not sure if this is a hint to my issue or not.

Does anyone have an idea why my STANDBY mode is not working and resetting the processor?

Thanks!

#stm32-stm32f103-reset-standby
This topic has been closed for replies.