STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OV7670 and DCMI problem

Posted on July 27, 2014 at 05:18I have been trying to get the OV7670 cam working with STM32F207zg but seems like something is not clear , first i need to know what is the buffer size to set the DMA to when i want to transfer a snapshot from the cam ...

TIM8 Toggle STM32F4

Posted on June 26, 2015 at 12:32 Hi, I'm trying to toggle some pins when timer 8 overflows. The problem I get is that I don´t see the pins toogle but I can see the timer counting on the debugger, so I think I might be missing some ...

pedro by Associate II
  • 1437 Views
  • 3 replies
  • 0 kudos

STM32F4 getting values from buffer

Posted on July 01, 2015 at 18:07 Hi, I wanted to personalize this code I found to fill half a buffer and then process the data while the second half of the buffer continues to fill. To understand how this works I modified the code so it turns on...

fiulala by Associate II
  • 895 Views
  • 2 replies
  • 0 kudos

STM32F103RF Dual Boot Problem

Posted on July 01, 2015 at 16:43 Hi, I am using STM32F103RF (XL density) micro and want to use the flash banks for firmware update. I took ''FLASH\Dual_Boot'' project of STM32F10x_StdPeriphLib as an example. My design is like that: I...

vcelik by Associate II
  • 1053 Views
  • 1 replies
  • 0 kudos

stm32 GNU ARM linker

Posted on June 30, 2015 at 11:27HiI am working with stm32 using GNU ARM Eclipse plugin.I want to modify the linker scripts to change the program start addressCan anyone help me?  Thanks

Cesar cfg by Associate II
  • 4160 Views
  • 10 replies
  • 0 kudos

STM32F411 - DMA only works once

Posted on April 12, 2015 at 18:59 Hi, I'm trying to use an STM32F411 Nucleo (Nucleo-F411RE) to drive a few Adafruit Neopixel LEDs (also known by the part number WS2812). These use a digital pseudo-PWM control signal to transfer digital d...

philpem by Associate II
  • 1885 Views
  • 2 replies
  • 0 kudos

STM32F091 CAN Filter Setup

Posted on June 29, 2015 at 21:20Hi, I'm using HAL functions for F0 and F1 to setup CAN filters to allow message only with global id (here is 0) and node id(here is 0x02) to be received. The F1(STM32F103CB) is working fine, but F0(STM32F091CC) only r...

Junbo Yi by Associate
  • 1152 Views
  • 1 replies
  • 0 kudos

STM32F405RGTx_FLASH.ld uses unaligned SP

Posted on June 01, 2015 at 08:51 Hello ST People, The .ld file that the cube generates for me (STM32F405RGTx_FLASH.ld) contains: _estack = 0x2001FFFF;    /* end of RAM */ but this makes the initial SP unaligned which I only noticed because some floa...

markb by Associate II
  • 1511 Views
  • 5 replies
  • 0 kudos